This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: TRNG

Part Number: CC1310

HI,

我使用的CC1310  2.40的SDK,程序中使用TRNG时,TRNGConfigure 配置MIN_REFILL_CYCLES 为1    MAX_REFILL_CYCLES为1  ,SMPL_DIV 为0, 产生的随机数是否从64到256?但是 实际debug发现产生的数值  TRNG_LOW_WORD大于256。是哪里配置不对吗

Power_setDependency(PowerCC26XX_PERIPH_TRNG);

TRNGConfigure(64,256,0);

TRNGEnable();

while (!(TRNGStatusGet() & TRNG_NUMBER_READY)) {

// Task_sleep(100);
}

bar = TRNGNumberGet(TRNG_LOW_WORD);

TRNGDisable();

Power_releaseDependency(PowerCC26XX_PERIPH_TRNG);

谢谢