Part Number: CC1125
Other Parts Discussed in Thread: CC1120
CC1125的原理图和手册差不多,测量输出信号会发现有频偏
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
CC1125在测量输出信号时发现频偏,可能是由于多种因素导致的,包括但不限于寄存器配置、晶振差异、外部环境干扰等。
首先,寄存器配置可能是一个关键因素。CC1125的寄存器设置对其输出频率有直接影响。如果寄存器配置不正确,或者与期望的频率设置不匹配,就可能导致输出信号存在频偏。因此,建议仔细检查CC1125的寄存器配置,确保它们与所需的输出频率一致。
其次,晶振的差异也可能导致频偏。虽然CC1125与某些其他RF芯片(如CC1120)在硬件上可能相似,但它们的晶振要求可能不同。如果更换了不同频率的晶振而没有相应地调整寄存器设置,就可能导致输出频率偏离预期。因此,在更换晶振时,务必确保按照手册要求进行调整。
此外,外部环境干扰也可能对CC1125的输出频率产生影响。例如,电磁干扰、温度变化等因素都可能导致频率偏移。为了减小这种影响,可以采取适当的屏蔽措施、优化PCB布局和布线、以及确保稳定的供电电压等。
最后,如果以上因素都排除了,但频偏问题仍然存在,可能需要考虑CC1125芯片本身的质量问题。