This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RSSI的精度(一致性)问题,以后会不会得到业界(尤其是Ti)更好地解决?

Other Parts Discussed in Thread: CC1000, CC2530

从CC1000芯片+6dB的“RSSI accuracy”到CC2530芯片+4dB的“Absolute uncalibrated RSSI/CCA accuracy”,看起来RSSI的不一致性问题在逐渐得到改善(数据源自CC1000和CC2530的datasheet)。

虽然RSSI的绝对值一直是一种不受待见的粗放型指示量,但能做的精确起来的话,应该能产生更多的效益。

毕竟对着同一信号,一个报-70dBm的强度,另一个报-60dBm的强度,还是非常不利于应用的。

芯片,外围电路,和天线三者应该共同影响着RSSI的精度(一致性),TI对芯片和外围电路用力很深

请问专家,业界以及TI有没有进一步解决这一问题的想法?

谢谢答复!