This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101接收其他433mhz芯片发射数据收不到

Other Parts Discussed in Thread: CC1101

TI技术人员您好,最近在使用贵公司的CC1101芯片作为接收端,发射端位英飞凌的SP370芯片,SP370集成了433.92mhz的发射器,设置为FSK方式,波特率9600,偏移±35kHz。CC1101也设置为2FSK的方式,使用smartrf设置的寄存器,中心频点也是433.92MHZ,9600波特率以及偏移35khz。却接收不到数据,想请问一下,我还需要设置一下哪些参数,如果想实现通信是否协议需要遵循。

此图为SP37,RFTX寄存器,设置为0x47(0100 0111B),关于发射方式以及频率的设置

以及RFENC寄存器,值为0xE0(1110 0000B),设置编码方式的寄存器。

以及通过smartRF相关寄存器的设置。


以下为检测到的信号频谱,前两张为SP370芯片频谱,后两张是通过以上寄存器设置,CC1101发射的寄存器频谱图像,从两者的频谱图像来看,不相同,应该是哪里设置的还是有问题。

以上SP30频谱图像

对应的,CC1101在相同档位下测到的频谱图像。