This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 多对设备同一空间中,在High Speed Mode下以约3.2mbps速率进行连续的数据传输是否可以实现?

Part Number: CC1310

像标题所说的我希望多组设备一对一传输,多个发送端放在一起,多个接收端放在一起(在同一块电路板的尺度上),在High Speed Mode下以约3.2mbps速率进行连续的数据传输,

1:我想了解这种使用情况是否能稳定传输;2:我该如何减少每组设备间的干扰;

我了解到在使用High Speed Mode模式时是8-fsk,3:那么他的信号带宽bw是多少,我该如何使用rfpacketER例程来调整SmartRF_settings中的相关参数来使用hsm呢。

注意到hsm下有效数据速率取决于数据包中的有效数据长度,4:比如我需要有效数据长度达到800字节需要使用advanced packet format,我该调整那些参数。