Other Parts Discussed in Thread: CC1101
两个CC1101芯片,一个收一个发,如何在发送端发射功率不变的情况下通过改变接收端的电路减小他俩之间的通信距离?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
天线不匹配,比如用的不是433MHz的天线,射频延长线的长度设计不对都会导致通信距离减小。
CC1101有一个衰减寄存器。可以增加一些衰减在接收端。FIFOTHR 【5.6】
CLOSE_IN_RX [1:0] 0 (00) R/W For more details, please see DN010 [11]
Setting RX Attenuation, Typical Values
0 (00) 0dB
1 (01) 6dB
2 (10) 12dB
3 (11) 18dB