做一个低功耗的433MHz无线测温项目,选择的发送芯片是cc1110,接受芯片是处理器加cc1101,实际测量过程中发现通讯距离还短了,完全达不到设计要求!!!距离大概也就30米左右的样子,请问专家们是怎么回事呢,是不是我在这个项目中选择的芯片有问题呢?测试条件是这样的:在空旷的大车间里,车间两头大概是50米的样子,无线模块放在桌子上,桌子大概50cm高度。芯片参数是:250kbps,安装ti推荐的高速参数设置的。天线:天线是网上买的3db增益的棒状天线。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
做一个低功耗的433MHz无线测温项目,选择的发送芯片是cc1110,接受芯片是处理器加cc1101,实际测量过程中发现通讯距离还短了,完全达不到设计要求!!!距离大概也就30米左右的样子,请问专家们是怎么回事呢,是不是我在这个项目中选择的芯片有问题呢?测试条件是这样的:在空旷的大车间里,车间两头大概是50米的样子,无线模块放在桌子上,桌子大概50cm高度。芯片参数是:250kbps,安装ti推荐的高速参数设置的。天线:天线是网上买的3db增益的棒状天线。
自己调试了一个月了没什么进展,天线是网上买的3dbi的,天线阻抗不知道怎么调?速度设置为38.4Kbps的了,调制方式为GFSK,输出功率是+10DB,距离可以达到大概40米的样子,CC1101接受时的RSSI大概在-73db左右。我把我的研发资料发给您,请您帮忙看看,在公司最近搞这个压力很大!资料有自己画的PCB板,还有做成的产品测试图片。
你有什么仪器?我看看你能测什么。
另外,频偏调过吗?
-73差不多了。但这个信号强度应该是可以正常解调的。
你的layout方面,crystal和走线下面最好是完整的地。电源线从外面绕才对。
BR.AZ
是可以解调,但是再稍微远几米就不可以了,信号强度就九十多了,layout我是参考TI的设计做的,TI有一个电源线是穿过CRYSTAL的,材料也是按照TI推荐的,推荐的晶振两边的电容值不一样,差个3pF。我只有示波器,我用示波器查看发射时候的电流,跟手册上介绍的差不多。对于频偏不知道怎么调?还有想请教的,就是我的项目需要400米的稳定距离,按照你们的专业经验,采用你们的CC1110+CC1101芯片最终是不是能够实现啊?
1110+1101怪怪的。
为啥不是msp430+1101.
400米是要看环境和速率的。
你会用频谱仪吗?可以约一下一些开放实验室,去测一下吧。
BR. AZ