This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 关于高空速下,WOR参数的配置问题

Part Number: CC1310

如标题,我目前使用WOR模式通信,在168K空速,WOR周期为4000ms时间的情况下会出现丢包的情况,而当我将WOR周期时间调小到2000ms或者500ms时,接收效果明显提升,目前对于RF_cmdPropRxSniff的配置如下所示,请问我应该怎么调整我的哪些参数,使其在4000ms时间下能减少丢包。

#define WOR_WAKE_UP_MARGIN_MS 5

#define CMD_PROP_RX_SNIFF                                       0x3808


RF_cmdPropRxSniff.startTime += (RFEnv.wor.recv_period_ms - WOR_WAKE_UP_MARGIN_MS) * 4000UL;

RF_cmdPropRxSniff.commandNo = CMD_PROP_RX_SNIFF; // Change to RX_SNIFF command from RX command

/* enalbe RSSI and PQT */
RF_cmdPropRxSniff.csConf.bEnaRssi = 0; /* Enable RSSI */
RF_cmdPropRxSniff.csConf.bEnaCorr = 1; /* Enable PQT */

/* General Carrier Sense configuration */
RF_cmdPropRxSniff.csConf.operation = 0; /* Busy if both RSSI and correlation indicates Busy */
RF_cmdPropRxSniff.csConf.busyOp = 0; /* Continue carrier sense on channel Busy */
RF_cmdPropRxSniff.csConf.idleOp = 1; /* End on channel Idle */
RF_cmdPropRxSniff.csConf.timeoutRes = 1; /* If the channel is invalid, it will return PROP_DONE_IDLE_TIMEOUT */

/* RSSI configuration */
RF_cmdPropRxSniff.numRssiIdle = 1; /* One idle RSSI samples signals that the channel is idle */
RF_cmdPropRxSniff.numRssiBusy = 1; /* One busy RSSI samples signals that the channel is busy */
RF_cmdPropRxSniff.rssiThr = (int8_t)WOR_RSSI_THRESHOLD; /* Set the RSSI threshold in dBm */

/* PQT configuration */
RF_cmdPropRxSniff.corrConfig.numCorrInv = 1; /* One busy PQT samples signals that the channel is busy */
RF_cmdPropRxSniff.corrConfig.numCorrBusy = 1; /* One busy PQT samples signals that the channel is busy */

/* Calculate basic timing parameters */
INT32U symbolLengthUs = 1000000UL / radio_rate; // radio period unit microsecond.
INT32U preambleSymbols = (wakeup_period_ms * 1000UL) / symbolLengthUs; // the number of preamble symbols.
INT8U syncWordSymbols = RF_cmdPropRadioDivSetup.formatConf.nSwBits; // the number of sync words.

/* Calculate sniff mode parameters */
#define US_TO_RAT_TICKS 4
#define CORR_PERIOD_SYM_MARGIN 8//16
#define RX_END_TIME_SYM_MARGIN 8
#define CS_END_TIME_MIN_TIME_SYM 30
#define CS_END_TIME_MIN_TIME_STATIC_US 150

/* Represents the time in which we need to receive corrConfig.numCorr* correlation peaks to detect preamble.
* When continously checking the preamble quality, this period has to be wide enough to also contain the sync
* word, with a margin. If it is not, then there is a chance the SNIFF command will abort while receiving the
* sync word, as it no longer detects a preamble. */
INT32U correlationPeriodUs = (syncWordSymbols + CORR_PERIOD_SYM_MARGIN)*symbolLengthUs;

/* Represents the time where we will force a check if preamble is present (only done once).
* The main idea is that his should be shorter than "correlationPeriodUs" so that if we get RSSI valid, but
* there is not a valid preamble on the air, we will leave RX as quickly as possible. */
INT32U csEndTimeUs = (CS_END_TIME_MIN_TIME_SYM*symbolLengthUs + CS_END_TIME_MIN_TIME_STATIC_US);

/* Represents the maximum time from the startTrigger to when we expect a sync word to be received. */
INT32U rxEndTimeUs = (preambleSymbols + syncWordSymbols + RX_END_TIME_SYM_MARGIN)*symbolLengthUs;

/* Set sniff mode timing configuration in sniff command in RAT ticks */
RF_cmdPropRxSniff.corrPeriod = (uint16_t)(correlationPeriodUs * US_TO_RAT_TICKS);
RF_cmdPropRxSniff.csEndTime = (INT32U)(csEndTimeUs * US_TO_RAT_TICKS);
RF_cmdPropRxSniff.endTime = (INT32U)(rxEndTimeUs * US_TO_RAT_TICKS);

/* Set correct trigger types */
RF_cmdPropRxSniff.csEndTrigger.triggerType = TRIG_REL_START; // carrier sense time from command started to csEndTimeUs.
RF_cmdPropRxSniff.endTrigger.triggerType = TRIG_REL_START; // maximum time from command startd to rxEndTimeUs.
RF_cmdPropRxSniff.startTrigger.triggerType = TRIG_ABSTIME; // sinff trigger use absolute time refer to radio RAT.
RF_cmdPropRxSniff.startTrigger.pastTrig = 1;

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 您好,

         如果您想每 4000 毫秒唤醒一次,这意味着您的发射器需要传输一个 4000 毫秒长的前导码。它能做到这一点吗?

         tramsitter 的前导码长度是确定 RX 端的 sniff 间隔的唯一因素。

         如果您查看 SDK 中的 WOR 示例,您将看到在 TX 端,前导码长度设置为 500 毫秒:      

    #define WOR_WAKEUPS_PER_SECOND 2
    
    /* WOR Example configuration defines */
    #define WOR_PREAMBLE_TIME_RAT_TICKS(x) \
        ((uint32_t)(4000000*(1.0f/(x))))
    
    RF_cmdPropTxAdv.preTime = WOR_PREAMBLE_TIME_RAT_TICKS(WOR_WAKEUPS_PER_SECOND);

    RX 的sniff interval配置为相同的

    #define WOR_WAKEUPS_PER_SECOND  2
    
    #define WOR_WAKE_UP_INTERVAL_RAT_TICKS(x) \
        ((uint32_t)(4000000*(1.0f/(x) - (WOR_WAKE_UP_MARGIN_S))))
        
    RF_cmdPropRxSniff.startTime += WOR_WAKE_UP_INTERVAL_RAT_TICKS(WOR_WAKEUPS_PER_SECOND);

    如果不更改 TX 则无法更改 RX

  • TX端那边,我修改了preTime,这里wakeup_period_ms是4000。

    RF_cmdPropTxAdv.preTrigger.triggerType = TRIG_REL_START;
    RF_cmdPropTxAdv.preTime = wakeup_period_ms * 4000UL;

  • 我这边想知道的就是,可能因为晶振或者PA这些外部原因,导致模块在时间上可能会有一些变化,比如我设置的1000ms,实际使用中是1001ms或是999ms。在我发的这些配置参数里面,对于这些比较小的改动,我应该调整哪些参数来进行匹配我当前的硬件

  • 您好,

         请参考下面的示例,它使用 168 kbps 的嗅探模式,传输 4 秒长的前导码。

    附加了设置、RX 和 TX 代码。

    您应该使用 SDK 中的 WoR 示例作为起点,然后替换与您共享的 3 个文件。

    不同时间的计算在我所附的单词 doument 中进行了解释。

    希望这有帮助。

    //*********************************************************************************
    // Generated by SmartRF Studio version 2.31.0 (build#400)
    // The applied template is compatible with CC13x0 SDK version 2.10.xx.xx or newer.
    // Device: CC1310 Rev. B (2.1).
    //
    //*********************************************************************************
    
    
    //*********************************************************************************
    // Parameter summary
    // RX Address0: 0xAA
    // RX Address1: 0xBB
    // RX Address Mode: No address check
    // Frequency: 868.00000 MHz
    // Data Format: Serial mode disable 
    // Deviation: 70.000 kHz
    // Packet Length Config: Variable 
    // Max Packet Length: 255 
    // Packet Length: 20
    // Packet Data: 255 
    // RX Filter BW: 311.0 kHz
    // Symbol Rate: 167.99927 kBaud
    // Sync Word Length: 32 Bits 
    // TX Power: 14 dBm (requires define CCFG_FORCE_VDDR_HH = 1 in ccfg.c, see CC13xx/CC26xx Technical Reference Manual)
    // Whitening: No whitening 
    
    #include "smartrf_settings.h"
    
    #include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_genfsk.h)
    #include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_genfsk.h)
    #include DeviceFamily_constructPath(inc/hw_rfc_dbell.h)
    
    // TI-RTOS RF Mode Object
    RF_Mode RF_prop =
    {
        .rfMode = RF_MODE_PROPRIETARY_SUB_1,
        .cpePatchFxn = &rf_patch_cpe_genfsk,
        .mcePatchFxn = 0,
        .rfePatchFxn = &rf_patch_rfe_genfsk
    };
    
    
    // Overrides for CMD_PROP_RADIO_DIV_SETUP
    uint32_t pOverrides[] =
    {
        // override_use_patch_prop_genfsk.xml
        // PHY: Use MCE ROM bank 4, RFE RAM patch
        MCE_RFE_OVERRIDE(0,4,0,1,0,0),
        // override_synth_prop_863_930_div5.xml
        // Synth: Set recommended RTRIM to 7
        HW_REG_OVERRIDE(0x4038,0x0037),
        // Synth: Set Fref to 4 MHz
        (uint32_t)0x000684A3,
        // Synth: Configure fine calibration setting
        HW_REG_OVERRIDE(0x4020,0x7F00),
        // Synth: Configure fine calibration setting
        HW_REG_OVERRIDE(0x4064,0x0040),
        // Synth: Configure fine calibration setting
        (uint32_t)0xB1070503,
        // Synth: Configure fine calibration setting
        (uint32_t)0x05330523,
        // Synth: Set loop bandwidth after lock to 20 kHz
        (uint32_t)0x0A480583,
        // Synth: Set loop bandwidth after lock to 20 kHz
        (uint32_t)0x7AB80603,
        // Synth: Configure VCO LDO (in ADI1, set VCOLDOCFG=0x9F to use voltage input reference)
        ADI_REG_OVERRIDE(1,4,0x9F),
        // Synth: Configure synth LDO (in ADI1, set SLDOCTL0.COMP_CAP=1)
        ADI_HALFREG_OVERRIDE(1,7,0x4,0x4),
        // Synth: Use 24 MHz XOSC as synth clock, enable extra PLL filtering
        (uint32_t)0x02010403,
        // Synth: Configure extra PLL filtering
        (uint32_t)0x00108463,
        // Synth: Increase synth programming timeout (0x04B0 RAT ticks = 300 us)
        (uint32_t)0x04B00243,
        // override_synth_disable_bias_div5.xml
        // Synth: Set divider bias to disabled
        HW32_ARRAY_OVERRIDE(0x405C,1),
        // Synth: Set divider bias to disabled (specific for loDivider=5)
        (uint32_t)0x18000200,
        // override_phy_rx_aaf_bw_0x0.xml
        // Rx: Set anti-aliasing filter bandwidth to 0x0 (in ADI0, set IFAMPCTL3[7:4]=0x0)
        ADI_HALFREG_OVERRIDE(0,61,0xF,0x0),
        // override_phy_gfsk_rx.xml
        // Rx: Set LNA bias current trim offset to 3
        (uint32_t)0x00038883,
        // Rx: Freeze RSSI on sync found event
        HW_REG_OVERRIDE(0x6084,0x35F1),
        // override_phy_gfsk_pa_ramp_5us_agc_reflevel_0x1c.xml
        // Tx: Configure PA ramping setting (0x10) for approximately 5 us PA ramp time. Rx: Set AGC reference level to 0x1C.
        HW_REG_OVERRIDE(0x6088,0x101C),
        // Tx: Configure PA ramping setting (0x08) for approximately 5 us PA ramp time
        HW_REG_OVERRIDE(0x608C,0x0813),
        // override_phy_rx_rssi_offset_5db.xml
        // Rx: Set RSSI offset to adjust reported RSSI by +5 dB (default: 0), trimmed for external bias and differential configuration
        (uint32_t)0x00FB88A3,
        // TX power override
        // Tx: Set PA trim to max (in ADI0, set PACTL0=0xF8)
        ADI_REG_OVERRIDE(0,12,0xF8),
    
        (uint32_t)0xFFFFFFFF
    };
    
    
    // CMD_PROP_RADIO_DIV_SETUP
    // Proprietary Mode Radio Setup Command for All Frequency Bands
    rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup =
    {
        .commandNo = 0x3807,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
        .startTime = 0x00000000,
        .startTrigger.triggerType = 0x0,
        .startTrigger.bEnaCmd = 0x0,
        .startTrigger.triggerNo = 0x0,
        .startTrigger.pastTrig = 0x0,
        .condition.rule = 0x1,
        .condition.nSkip = 0x0,
        .modulation.modType = 0x1,
        .modulation.deviation = 0x118,
        .symbolRate.preScale = 0xF,
        .symbolRate.rateWord = 0x1AE14,
        .symbolRate.decimMode = 0x0,
        .rxBw = 0x29,
        .preamConf.nPreamBytes = 0x4,
        .preamConf.preamMode = 0x0,
        .formatConf.nSwBits = 0x20,
        .formatConf.bBitReversal = 0x0,
        .formatConf.bMsbFirst = 0x1,
        .formatConf.fecMode = 0x0,
        .formatConf.whitenMode = 0x0,
        .config.frontEndMode = 0x0,
        .config.biasMode = 0x1,
        .config.analogCfgMode = 0x0,
        .config.bNoFsPowerUp = 0x0,
        .txPower = 0xA73F,
        .pRegOverride = pOverrides,
        .centerFreq = 0x0364,
        .intFreq = 0x8000,
        .loDivider = 0x05
    };
    
    
    // CMD_FS
    // Frequency Synthesizer Programming Command
    rfc_CMD_FS_t RF_cmdFs =
    {
        .commandNo = 0x0803,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
        .startTime = 0x00000000,
        .startTrigger.triggerType = 0x0,
        .startTrigger.bEnaCmd = 0x0,
        .startTrigger.triggerNo = 0x0,
        .startTrigger.pastTrig = 0x0,
        .condition.rule = 0x1,
        .condition.nSkip = 0x0,
        .frequency = 0x0364,
        .fractFreq = 0x0000,
        .synthConf.bTxMode = 0x0,
        .synthConf.refFreq = 0x0,
        .__dummy0 = 0x00,
        .__dummy1 = 0x00,
        .__dummy2 = 0x00,
        .__dummy3 = 0x0000
    };
    
    
    // CMD_PROP_TX
    // Proprietary Mode Transmit Command
    rfc_CMD_PROP_TX_t RF_cmdPropTx =
    {
        .commandNo = 0x3801,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
        .startTime = 0x00000000,
        .startTrigger.triggerType = 0x0,
        .startTrigger.bEnaCmd = 0x0,
        .startTrigger.triggerNo = 0x0,
        .startTrigger.pastTrig = 0x0,
        .condition.rule = 0x1,
        .condition.nSkip = 0x0,
        .pktConf.bFsOff = 0x0,
        .pktConf.bUseCrc = 0x1,
        .pktConf.bVarLen = 0x1,
        .pktLen = 0x14,
        .syncWord = 0x930B51DE,
        .pPkt = 0 // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    };
    
    
    // CMD_PROP_RX
    // Proprietary Mode Receive Command
    rfc_CMD_PROP_RX_t RF_cmdPropRx =
    {
        .commandNo = 0x3802,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
        .startTime = 0x00000000,
        .startTrigger.triggerType = 0x0,
        .startTrigger.bEnaCmd = 0x0,
        .startTrigger.triggerNo = 0x0,
        .startTrigger.pastTrig = 0x0,
        .condition.rule = 0x1,
        .condition.nSkip = 0x0,
        .pktConf.bFsOff = 0x0,
        .pktConf.bRepeatOk = 0x0,
        .pktConf.bRepeatNok = 0x0,
        .pktConf.bUseCrc = 0x1,
        .pktConf.bVarLen = 0x1,
        .pktConf.bChkAddress = 0x0,
        .pktConf.endType = 0x0,
        .pktConf.filterOp = 0x0,
        .rxConf.bAutoFlushIgnored = 0x0,
        .rxConf.bAutoFlushCrcErr = 0x0,
        .rxConf.bIncludeHdr = 0x1,
        .rxConf.bIncludeCrc = 0x0,
        .rxConf.bAppendRssi = 0x0,
        .rxConf.bAppendTimestamp = 0x0,
        .rxConf.bAppendStatus = 0x1,
        .syncWord = 0x930B51DE,
        .maxPktLen = 0xFF,
        .address0 = 0xAA,
        .address1 = 0xBB,
        .endTrigger.triggerType = 0x1,
        .endTrigger.bEnaCmd = 0x0,
        .endTrigger.triggerNo = 0x0,
        .endTrigger.pastTrig = 0x0,
        .endTime = 0x00000000,
        .pQueue = 0, // INSERT APPLICABLE POINTER: (dataQueue_t*)&xxx
        .pOutput = 0 // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
    };

    /*
     * Copyright (c) 2016-2019, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     */
    
    /***** Includes *****/
    /* Standard C Libraries */
    #include <stdlib.h>
    
    /* XDCtools Header files */
    #include <xdc/std.h>
    #include <xdc/runtime/Assert.h>
    
    /* BIOS Header files */
    #include <ti/sysbios/BIOS.h>
    #include <ti/sysbios/knl/Task.h>
    
    /* TI-RTOS Header files */
    #include <ti/drivers/rf/RF.h>
    #include <ti/drivers/PIN.h>
    #include <ti/drivers/pin/PINCC26XX.h>
    
    /* Board Header files */
    #include "Board.h"
    
    /* Application Header files */
    #include "RFQueue.h"
    #include "smartrf_settings/smartrf_settings.h"
    
    #include <ti/devices/DeviceFamily.h>
    #include DeviceFamily_constructPath(driverlib/rf_prop_mailbox.h)
    
    /* TI-RTOS Task configuration */
    #define RX_TASK_STACK_SIZE 1024
    #define RX_TASK_PRIORITY   2
    
    /* TX Configuration */
    #define DATA_ENTRY_HEADER_SIZE 8  /* Constant header size of a Generic Data Entry */
    #define MAX_LENGTH             31 /* Max length byte the radio will accept */
    #define NUM_DATA_ENTRIES       2  /* NOTE: Only two data entries supported at the moment */
    #define NUM_APPENDED_BYTES     1  /* Length byte included in the stored packet */
    
    #define CS_END_TIME         923
    #define CORR_PERIOD         1167
    #define END_TIME            16002583
    
    #define SNIFF_INTERVAL (uint32_t)(4000000*(3.9998095f));
    
    
    
    /***** Variable declarations *****/
    /* TX task objects and task stack */
    static Task_Params rxTaskParams;
    static Task_Struct rxTask;
    static uint8_t rxTaskStack[RX_TASK_STACK_SIZE];
    
    /* RF driver object and handle */
    static RF_Object rfObject;
    static RF_Handle rfHandle;
    
    /* Pin driver object and handle */
    static PIN_Handle ledPinHandle;
    static PIN_State ledPinState;
    
    static PIN_Config pinTable[] =
    {
        Board_PIN_LED0 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
        Board_PIN_LED1 | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
    	PIN_TERMINATE
    };
    
    /* Buffer which contains all Data Entries for receiving data.
     * Pragmas are needed to make sure this buffer is 4 byte aligned (requirement from the RF Core) */
    #if defined(__TI_COMPILER_VERSION__)
        #pragma DATA_ALIGN (rxDataEntryBuffer, 4);
            static uint8_t rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
                                                                     MAX_LENGTH,
                                                                     NUM_APPENDED_BYTES)];
    #elif defined(__IAR_SYSTEMS_ICC__)
        #pragma data_alignment = 4
            static uint8_t rxDataEntryBuffer[RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
                                                                     MAX_LENGTH,
                                                                     NUM_APPENDED_BYTES)];
    #elif defined(__GNUC__)
            static uint8_t rxDataEntryBuffer [RF_QUEUE_DATA_ENTRY_BUFFER_SIZE(NUM_DATA_ENTRIES,
                MAX_LENGTH, NUM_APPENDED_BYTES)] __attribute__ ((aligned (4)));
    #else
        #error This compiler is not supported.
    #endif
    
    /* RX Data Queue and Data Entry pointer to read out received packets */
    static dataQueue_t dataQueue;
    static rfc_dataEntryGeneral_t* currentDataEntry;
    
    /* Received packet's length and pointer to the payload */
    static uint8_t packetLength;
    static uint8_t* packetDataPointer;
    
    static volatile uint8_t dummy;
    
    rfc_propRxOutput_t rxStatistics;
    
    /* Sniff command for doing combined Carrier Sense and RX*/
    static rfc_CMD_PROP_RX_SNIFF_t RF_cmdPropRxSniff;
    
    /***** Prototypes *****/
    static void rxTaskFunction(UArg arg0, UArg arg1);
    static void callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e);
    
    /***** Function definitions *****/
    /* RX task initialization function. Runs once from main() */
    void rxTaskInit()
    {
        Task_Params_init(&rxTaskParams);
        rxTaskParams.stackSize = RX_TASK_STACK_SIZE;
        rxTaskParams.priority = RX_TASK_PRIORITY;
        rxTaskParams.stack = &rxTaskStack;
    
        Task_construct(&rxTask, rxTaskFunction, &rxTaskParams, NULL);
    }
    
    /* RX task function. Executed in Task context by TI-RTOS when the scheduler starts. */
    static void rxTaskFunction(UArg arg0, UArg arg1)
    {
        RF_Params rfParams;
        RF_Params_init(&rfParams);
    
        /* Create queue and data entries */
        if (RFQueue_defineQueue(&dataQueue,
                                rxDataEntryBuffer,
                                sizeof(rxDataEntryBuffer),
                                NUM_DATA_ENTRIES,
                                MAX_LENGTH + NUM_APPENDED_BYTES))
        {
            /* Failed to allocate space for all data entries */
            while(1);
        }
    
        // Copy RX configuration from RX command
        memcpy(&RF_cmdPropRxSniff, &RF_cmdPropRx, sizeof(rfc_CMD_PROP_RX_t));
    
        // Change to RX_SNIFF command from RX command
        RF_cmdPropRxSniff.commandNo                 = CMD_PROP_RX_SNIFF;
        RF_cmdPropRxSniff.startTrigger.triggerType  = TRIG_ABSTIME;
        RF_cmdPropRxSniff.startTrigger.pastTrig     = 0;
        RF_cmdPropRxSniff.rxConf.bAutoFlushIgnored  = 1; // Discard ignored packets from Rx queue
        RF_cmdPropRxSniff.rxConf.bAutoFlushCrcErr   = 1; // Discard packets with CRC error from Rx queue
        RF_cmdPropRxSniff.maxPktLen                 = MAX_LENGTH; // Implement packet length filtering to avoid PROP_ERROR_RXBUF
        RF_cmdPropRxSniff.endTrigger.triggerType    = TRIG_REL_START;
        RF_cmdPropRxSniff.endTime                   = END_TIME;
        RF_cmdPropRxSniff.pQueue                    = &dataQueue; // Set the Data Entity queue for received data
        RF_cmdPropRxSniff.pOutput                   = (uint8_t*)&rxStatistics;
        RF_cmdPropRxSniff.csConf.bEnaRssi           = 0; // Use RSSI to monitor the channel
        RF_cmdPropRxSniff.csConf.bEnaCorr           = 1; // Use the correlator as well as RSSI, to prevent too many false BUSY channels
        RF_cmdPropRxSniff.csConf.operation          = 1; // Only declare the channel BUSY if both the RSSI and CS criterion are met
        RF_cmdPropRxSniff.csConf.busyOp             = 0; // Continuously monitor the channel so that we can exit as soon as the channel state is IDLE
        RF_cmdPropRxSniff.csConf.idleOp             = 1; // Exit RX as soon as an IDLE channel is detected
        RF_cmdPropRxSniff.csConf.timeoutRes         = 1;
        RF_cmdPropRxSniff.rssiThr                   = (-90); // Used for demo purposes
        RF_cmdPropRxSniff.numRssiIdle               = 1;
        RF_cmdPropRxSniff.numRssiBusy               = 1;
        RF_cmdPropRxSniff.corrPeriod                = CORR_PERIOD;
        RF_cmdPropRxSniff.corrConfig.numCorrInv     = 1;
        RF_cmdPropRxSniff.corrConfig.numCorrBusy    = 1;
        RF_cmdPropRxSniff.csEndTrigger.triggerType  = TRIG_REL_START;
        RF_cmdPropRxSniff.csEndTime                 = CS_END_TIME;
    
        rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
    
        /* Set frequency */
        RF_runCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, &callback, 0);
    
        /* Save the current radio time */
        RF_cmdPropRxSniff.startTime = RF_getCurrentTime();
    
        /* Enter main loop */
        while(1)
        {
            RF_cmdPropRxSniff.startTime += SNIFF_INTERVAL;
    
            /* Schedule RX */
            RF_runCmd(rfHandle, (RF_Op*)&RF_cmdPropRxSniff, RF_PriorityNormal, &callback, RF_EventRxEntryDone);
        }
    }
    
    
    /* Called for every received packet and command done */
    void callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e)
    {
        /* If we've received a new packet and it's available to read out */
        if (e & RF_EventRxEntryDone)
        {
            do
            {
                /* Toggle LED on RX */
                PIN_setOutputValue(ledPinHandle, Board_PIN_LED0, !PIN_getOutputValue(Board_PIN_LED0));
    
                /* Get current unhandled data entry */
                currentDataEntry = RFQueue_getDataEntry();
    
                /* Handle the packet data, located at &currentDataEntry->data:
                 * - Length is the first byte with the current configuration
                 * - Data starts from the second byte */
                packetLength      = *(uint8_t*)(&currentDataEntry->data);
                packetDataPointer = (uint8_t*)(&currentDataEntry->data + 1);
    
                /* This code block is added to avoid a compiler warning.
                * Normally, an application will reference these variables for
                * useful data. */
                dummy = packetLength + packetDataPointer[0];
    
            } while(RFQueue_nextEntry() == DATA_ENTRY_FINISHED);
        }
    }
    
    
    /*
     *  ======== main ========
     */
    int main(void)
    {
        /* Call driver init functions. */
        Board_initGeneral();
    
        /* Open LED pins */
        ledPinHandle = PIN_open(&ledPinState, pinTable);
        Assert_isTrue(ledPinHandle != NULL, NULL);
    
        /* Initialize task */
        rxTaskInit();
    
        /* Start BIOS */
        BIOS_start();
    
        return (0);
    }

    cmdPropRxSniff.docx

    这个代码,测试传输 100 数据包没有丢失任何一个数据包

  • 这个docx进不去,提示You do not have permission to view this directory or page.

  • 您好,

           请直接测试代码。