我想通过信号源测试我的接收灵敏度,由于信号源只能发送0101码,因此我必须把前导码和同步字全部设置成0xAA或者0x55,但是我一旦全部设成0xAA或者0x55就无法正常通信,TI的工程师们能不能告诉我这是什么问题,是不是还别的寄存器需要设置?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想通过信号源测试我的接收灵敏度,由于信号源只能发送0101码,因此我必须把前导码和同步字全部设置成0xAA或者0x55,但是我一旦全部设成0xAA或者0x55就无法正常通信,TI的工程师们能不能告诉我这是什么问题,是不是还别的寄存器需要设置?
默认就是AA呀。。。。我觉得还是你的信号源的配置问题吧?
你有没有验证一下,用两个1125先对发验证一下?然后把所有的“1”“0”key到信号源里去。
BR. AZ
谢谢你的回答,这个问题我基本上已经解决了,我现在的问题是想把接到的数据通过CC125的GPIO3输出来,然后观察GPIO3的波形,该怎么做?
可参考user guide里面的GPIOx mapping部分。 BR. AZ