This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc1101不能接收的问题

Other Parts Discussed in Thread: CC1101

TI的各位专家:

有关CC1101的OOK/ASK模式收发有些问题请教一下,发送端一直在发,接收端间隔一定的时间去读数据,但是读的数据有问题,我怀疑是配置不对,

配置参考如下

halSpiWriteReg(CCxxx0_IOCFG2,0x0d);
halSpiWriteReg(CCxxx0_IOCFG1,0x2e);
halSpiWriteReg(CCxxx0_IOCFG0,0x08);
halSpiWriteReg(CCxxx0_FIFOTHR,0x47); //DN022 RX filter bandwidth ≤ 325 kHz
halSpiWriteReg(CCxxx0_SYNC1,0xD3);
halSpiWriteReg(CCxxx0_SYNC0,0x91);
halSpiWriteReg(CCxxx0_PKTLEN,0x20);
halSpiWriteReg(CCxxx0_ADDR,0x00);
halSpiWriteReg(CCxxx0_CHANNR,0x00);
halSpiWriteReg(CCxxx0_PKTCTRL0,0x32);
halSpiWriteReg(CCxxx0_FSCTRL1,0x06);
halSpiWriteReg(CCxxx0_FSCTRL0,0x00);
halSpiWriteReg(CCxxx0_FREQ2,0x10); //433.92MHz
halSpiWriteReg(CCxxx0_FREQ1,0xB0);
halSpiWriteReg(CCxxx0_FREQ0,0x71);
halSpiWriteReg(CCxxx0_MDMCFG4,0xbB);
halSpiWriteReg(CCxxx0_MDMCFG3,0x83); //76K RX filter bandwidth = 203 kHz
halSpiWriteReg(CCxxx0_MDMCFG2,0x30);
halSpiWriteReg(CCxxx0_MDMCFG1,0x42);
halSpiWriteReg(CCxxx0_MDMCFG0,0xf8);
halSpiWriteReg(CCxxx0_DEVIATN,0x15);
halSpiWriteReg(CCxxx0_MCSM2,0x07);
halSpiWriteReg(CCxxx0_MCSM1,0x30);
halSpiWriteReg(CCxxx0_MCSM0,0x18);
halSpiWriteReg(CCxxx0_FOCCFG,0x14);
halSpiWriteReg(CCxxx0_BSCFG,0x6C);
halSpiWriteReg(CCxxx0_AGCCTRL2, 0xff);
halSpiWriteReg(CCxxx0_AGCCTRL1, 0x00); //add mike
halSpiWriteReg(CCxxx0_AGCCTRL0, 0x91);
halSpiWriteReg(CCxxx0_WOREVT1, 0x43);
halSpiWriteReg(CCxxx0_WOREVT0, 0xB5); //add mike
halSpiWriteReg(CCxxx0_WORCTRL,0x68);
halSpiWriteReg(CCxxx0_FREND1,0xB6); //DN022 RX filter bandwidth > 101 kHz
halSpiWriteReg(CCxxx0_FREND0,0x11);
halSpiWriteReg(CCxxx0_FSCAL3,0xE9);
halSpiWriteReg(CCxxx0_FSCAL2,0x2A);
halSpiWriteReg(CCxxx0_FSCAL1,0x00);
halSpiWriteReg(CCxxx0_FSCAL0,0x1F);
halSpiWriteReg(CCxxx0_TEST2,0x81); //DN022 RX filter bandwidth ≤ 325 kHz
halSpiWriteReg(CCxxx0_TEST1,0x35); //DN022 RX filter bandwidth ≤ 325 kHz
halSpiWriteReg(CCxxx0_TEST0,0x09);
halSpiWriteReg(CCxxx0_RCCTRL1,0x41);
halSpiWriteReg(CCxxx0_RCCTRL0,0x00);
halSpiWriteReg(CCxxx0_FSTEST,0x59);
halSpiWriteReg(CCxxx0_PTEST,0x7F);

麻烦各位专家看一下,代码有不正确的也请帮忙指正。

期盼您的回复。

非常感谢!