我是使用Provisioning_smart_config这个例子,有些时候手机用smartconfig配置能成功,能看到红灯亮了,但是手机上一直都没有提示“new device found”,然后手机切入到devices中,不断更新也找不到,只有重新把手机的wifi starter 重新启动才能找到(只是偶尔能找到);请问怎样才能提高找到设备的成功率;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
因为有些路由器对于mDNS的支持不好,所以CC3200在发出MDNS的包,有时候会被drop掉,建议在开发的时候可以使用UDP广播来做。
您好,您说用provisioning_smartconfig的时候如若连接路由器成功,会开启mdns,但是我在程序中并没有找到register,只在初始化配置的时候看到了unregister,请问具体在哪里呢?
官方有一个mDNS的例子,我增加一些备注,可供参考
//*****************************************************************************
//
//! Main function
//!
//! \param None
//!
//! \return None
//!
// In SDK example device is advertising it's IP using mDNS protocol. You need to implement mDNS listener at the other end(mobile or PC) .
// You can easily implement mDNS listener as its very simple protocol. mDNS uses multicast UDP packets.
//
// 1. Create a udp socket on port 5353
// 2. Join muticast group on "224.0.0.251"
// 3. receive packets and parse the data retrieve IP
//
// For more details please go through mDNS RFC(rfc6762).
//
// sl_NetAppMDNSRegisterService()向 224.0.0.251 + 5353广播自己的IP地址和端口号及message
// sl_NetAppDnsGetHostByService()监听224.0.0.251 + 5353地址接收到提供服务的目的IP地址和端口号及message
//*****************************************************************************
static long mDNS_Task()
{
int iretvalmDNS;
long lRetVal = -1;
unsigned char policyVal;
#ifndef MDNS_ADVERTISE
unsigned int pAddr;
unsigned long usPort;
unsigned short ulTextLen = 200;
char cText[200];
int i;
#endif
InitializeAppVariables();
//
// Following function configure the device to default state by cleaning
// the persistent settings stored in NVMEM (viz. connection profiles &
// policies, power policy etc)
//
// Applications may choose to skip this step if the developer is sure
// that the device is in its default state at start of applicaton
//
// Note that all profiles and persistent settings that were done on the
// device will be lost
//
lRetVal = ConfigureSimpleLinkToDefaultState();
if(lRetVal < 0)
{
if (DEVICE_NOT_IN_STATION_MODE == lRetVal)
{
UART_PRINT("Failed to configure the device in its default state\n\r");
}
return -1;
}
UART_PRINT("Device is configured in default state \n\r");
//
// Assumption is that the device is configured in station mode already
// and it is in its default state
//
lRetVal = sl_Start(0, 0, 0);
if (lRetVal < 0 || ROLE_STA != lRetVal)
{
UART_PRINT("Failed to start the device \n\r");
return -1;
}
UART_PRINT("Device started as STATION \n\r");
//powering on the CC3200 device
//reset all policies
sl_WlanPolicySet( SL_POLICY_CONNECTION,
SL_CONNECTION_POLICY(0,0,0,0,0),
&policyVal,
1 /*PolicyValLen*/);
//
//Connecting to WLAN AP
//
lRetVal = WlanConnect();
ASSERT_ON_ERROR(lRetVal);
UART_PRINT("Connection established w/ AP and IP is aquired \n\r");
#ifdef MDNS_ADVERTISE
//Registering for the mDNS service.
iretvalmDNS = sl_NetAppMDNSUnRegisterService(SERVICE_NAME,(unsigned char)strlen(SERVICE_NAME));
// Time To Live(TTL)生存时间(in seconds),简单的说它表示DNS记录在DNS服务器上缓存时间
// Advertise(Mdns host) 向224.0.0.251 + 5353广播自己的IP地址和端口号及message
//--------------------------------------------------------------------mDNS服务理解---------------------------------------------------------------------------------
// CC3200_A连接AP进入局域网获取自身IP地址,同时开启mDNS服务,并向mDNS服务注册一下信息(sl_NetAppMDNSRegisterService):我提供SERVICE_NAME服务,我IP:192.168.1.101端口200
// 当CC3200_B连接AP进入局域网,并向CC3200_B的mDNS服务请求(sl_NetAppDnsGetHostByService),我要找局域网内SERVICE_NAME服务器,CC3200_B的mDNS就会去局域网内向其他的mDNS询问,
// 并且最终告诉你,有一个IP地址为192.168.1.101,端口号是200的主机,也就是CC3200_A提供SERVICE_NAME服务,所以CC3200_B就知道了CC3200_A的IP地址和端口号了。
//-----------------------------------------------------------------------------------------------------------------------------------------------------------------
iretvalmDNS = sl_NetAppMDNSRegisterService(SERVICE_NAME,(unsigned char)strlen(SERVICE_NAME),"Service registered for 3200",\
(unsigned char)strlen("Service registered for 3200"),200,2000,1); //端口号Port=200 + Time To Live(TTL)=2000 + service is unique
if(iretvalmDNS == 0)
{
Report("MDNS Registration successful\n\r");
}
else
{
Report("MDNS Registered failed\n\r");
}
#else
for( i= 0;i<100;i++)
{
iretvalmDNS = 1;
while(iretvalmDNS)
{
ulTextLen = 200;
// listen(Mdns client) 监听224.0.0.251 + 5353地址接收到提供服务的目的IP地址和端口号及message
iretvalmDNS = sl_NetAppDnsGetHostByService(SERVICE_NAME,(unsigned char)strlen(SERVICE_NAME),SL_AF_INET,(unsigned long *)&pAddr,&usPort,&ulTextLen,&cText[0]);
}
if(iretvalmDNS == 0)
{
cText[ulTextLen] = '\0';
Report("\n\rPort: %d\n\r",usPort );
Report("Addr: %d.%d.%d.%d\n\r",SL_IPV4_BYTE(pAddr,3),
SL_IPV4_BYTE(pAddr, 2), SL_IPV4_BYTE(pAddr, 1),
SL_IPV4_BYTE(pAddr, 0));
Report("TLen: %d\n\r",ulTextLen );
Report("Text: %s\n\r",cText );
}
}
#endif
return SUCCESS;
}