This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200自制PCB的ADC采集结果很奇怪!

Other Parts Discussed in Thread: CC3200

大家好!

我们自己画的PCB在使用adc例程的时候,采集结果很奇怪(用LaunchPad测试正常),采用的AD输入引脚是PIN_60,现象如下:

情况一,通过100k电阻接GND,输出的128个结果匀为4095。

情况二,通过100k电阻接GND,并联0.1uF电容一个,输出的128个结果由小变大,约从2500多增加到4095。

最小系统部分的原理图画法和LaunchPad一样,无线网络部分功能正常。

由表象看可能是芯片内部的AD输入端有电流输入,会不会可能是哪里的布线出现了问题?

附件为原理如,请下载。

Sheet1.PDF