This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc3200 RTC timer打断 sl_sendto



各位大神好,

我最近在用LDPS模式,所以在iddleprofile里修改了一下,用rtc 定时器来做UDP发送的定时器(开始把cc_idle_task_pm()函数屏蔽掉了,其实进不进LDPS都会出现这个问题)

我把发送任务放到大循环里,利用标志位每50ms发送一次,一开始发送任务可以进行,但是当发送了几百几千次(有时候是几十次,随机性很强)之后,sl_sendto停止发送,又经过几个循环之后,sl_sendto返回SL_EAGAIN(-11 手册上标注的try again),之后就一直返回-11.

如果换一个timer,比如timer0,timer1都没用这个问题。

SetTimerAsWkUp()是iddleprofile里原来就有的,创建唤醒定时器,SetTimerAsWkUp2()是我用论坛行看见的,把中间四句删掉(在timercallback里只是重设timer而不是重新创建)。这个RTC 的timer运行一直没问题,就是发送函数有问题。

void TimerCallback(void *vParam)
{
 
LPDS_Flag2=1;
SetTimerAsWkUp2();

}

cc_hndl SetTimerAsWkUp()
{
    cc_hndl tTimerHndl;
    struct cc_timer_cfg sRealTimeTimer;
    struct u64_time sInitTime, sIntervalTimer;
    //
    // setting up Timer as a wk up source and other timer configurations
    //
    sInitTime.secs = 0;
    sInitTime.nsec = 0;
    cc_rtc_set(&sInitTime);

    sRealTimeTimer.source = HW_REALTIME_CLK;
    sRealTimeTimer.timeout_cb = TimerCallback;
    sRealTimeTimer.cb_param = NULL;

    tTimerHndl = cc_timer_create(&sRealTimeTimer);

    sIntervalTimer.secs = LPDS_DUR_SEC;
    sIntervalTimer.nsec = LPDS_DUR_NSEC;
    cc_timer_start(tTimerHndl, &sIntervalTimer,OPT_TIME_ABS_VALUE);
    return(tTimerHndl);
}
cc_hndl SetTimerAsWkUp2()
{
    cc_hndl tTimerHndl;
    struct cc_timer_cfg sRealTimeTimer;
    struct u64_time sInitTime, sIntervalTimer;
    //
    // setting up Timer as a wk up source and other timer configurations
    //
    sInitTime.secs = 0;
    sInitTime.nsec = 0;
 
 cc_rtc_set(&sInitTime);
 
 /* 

    sRealTimeTimer.source = HW_REALTIME_CLK;
    sRealTimeTimer.timeout_cb = TimerCallback;
    sRealTimeTimer.cb_param = NULL;
 
   
    tTimerHndl = cc_timer_create(&sRealTimeTimer); */
    timer_created++;
    sIntervalTimer.secs = LPDS_DUR_SEC;
    sIntervalTimer.nsec = LPDS_DUR_NSEC;
    cc_timer_start(tTimerHndl, &sIntervalTimer,OPT_TIME_ABS_VALUE);
    return(tTimerHndl);
}


//udpclient main loop
while(1)
{
  if(LPDS_Flag2==1)
  {
  
 GPIO_IF_LedToggle(MCU_RED_LED_GPIO);  
iStatus= sl_SendTo( 0,  &wifi_send_buf, 1, 0,( SlSockAddr_t *)&sAddr_Flag, iAddrSize_Flag); 
GPIO_IF_LedToggle(MCU_RED_LED_GPIO);

 LPDS_Flag2=0;
 UART_PRINT("istatus is %d",iStatus);
 


  }
}

socket我设置成了nonblock模式

 sl_SetSockOpt(iSockID,SOL_SOCKET,SL_SO_NONBLOCKING, &enableOption,sizeof(enableOption));

如果不这样设置的话,从sl_sendto这里就直接阻塞了,调到idle task里面回不来了了