在例程MQTT Server中,是使用其中一块3200作为本地的服务器,其他的CC3200作为本地客户端。本地客户端可以通过本地服务器将数据上传到远端的服务器,同样也可以下载。我现在知道作为本地服务器的那块CC3200同时兼顾着和远端服务器通信和管理本地MQTT网络的功能,也可以使用它和远端服务器进行通信了。但是我现在不清楚怎么样才能将其他的板子和这块作为本地服务器的CC3200通过MQTT协议进行连接,然后进行本地通信。文档里面是这么说的,
8. Connect one or multiple local MQTT client to the MQTT server, it can be a PC or another CC3200 device. A
local functional MQTT network can now be used to communicate between multiple local clients.
这个local functional MQTT network应该怎么搭建起来呢?是需要本地服务器的那块CC3200的地址和端口吗?为什么在代码里面没有找到有对应的地方。麻烦TI工程师能指点一下。