This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200在2.8V以下不能正常工作

Other Parts Discussed in Thread: CC3200

       采用CC3200R1M2RGCR芯片自已画的模块,烧写Radio Tool中的Bin文件,使用Radio Tool工具测试时,发现3V供电时串口可以正常连接,WIFI的TX也可正常发数据。可是供电电压到2.8V,串口可以连接,但是WIFI 的TX没有数据发出。2.5V时,串口都连接不上了。

     原理图和PCB的设计都是参考了TI的参考设计的。3V供电系统和40M晶体都是正常的。请问我需要再查什么地方,谢谢!