This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc3100WiFi

Other Parts Discussed in Thread: MSP430F5529, CC3100

ti的老师你们好,我现在在用cc3100与mspf5529配合使用,想把msp430f5529单片机adc采样到的数字信号通过cc3100WiFi模块发送到电脑上,然后将该数据储存在电脑中。那我应该具体怎么实现呢?mspf5529与cc3100之间用spi通信,因为对于传输速度要求比较高!请ti的老师们给点思路。关于cc3100的基本文档和sdk我都看了,还是没有思路。非常感谢,请老师们指点下。

  • 1、CC3100作为Station模式,你电脑虚拟一个wifi热点/AP,将CC3100连接到这个虚拟wifi热点/AP进行数据传输

    2、CC3100作为Station模式,你电脑也作为Station模式,同时去连接一个路由器/AP,通过路由器/AP进行转发数据到你的电脑

    通过上述两种方法都可以讲ADC采集的数据发送到电脑中。

  • 老师您好,谢谢您的细心解答,我还有几个问题不太明白!想请教下您。

    1、在数据传输的过程中电脑需要什么软件将传输来的数据储存呢?

    2、我如果参照getting_started_with_wlan_station这个ti的例程的话,控制cc3100单片机程序需要更改什么地方的程序代码呢?才能将msp430f5529采集到的数据发送给cc3100.

    谢谢老师解答,刚刚接触cc3100,不是很明白!

  • 1、电脑一般使用TCP/UDP的上位机软件来接收数据,也可以自己写上位机软件来接收存储数据。

    2、例程中将AP名字改为你自己电脑虚拟的wifi名称及密码或者是路由器的名称及密码,当CC3100连接到AP、路由器后通过过目的IP地址及端口号就可以给电脑发送数据了,关于数据的采集及存储你可以自己写上位机进行特定功能的数据存储。

  • 好的,谢谢老师解答!