This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3100的station模式已经工作正常,但手机怎么向单片机发送信息呢,是用TCP协议吗?

Other Parts Discussed in Thread: CC3100, CC3200

RT

  • 1. CC3100连接到本地的路由器或者AP,手机也连接到本地的路由器或者AP上,在同一个局域网中连接好所有设备,通过建立TCP,UPD的方式,可以在手机端建立TCP或者UDP的服务器,用CC3100建立相应的客户端,通过指定的IP地址和端口号就可以通过手机发送数据信息到CC3100,CC3100可以通过串口UART或者SPI的方式传递给单片机,实现手机向单片机发送信息的过程。

  • Terry Han 说:

    1. CC3100连接到本地的路由器或者AP,手机也连接到本地的路由器或者AP上,在同一个局域网中连接好所有设备,通过建立TCP,UPD的方式,可以在手机端建立TCP或者UDP的服务器,用CC3100建立相应的客户端,通过指定的IP地址和端口号就可以通过手机发送数据信息到CC3100,CC3100可以通过串口UART或者SPI的方式传递给单片机,实现手机向单片机发送信息的过程。

    请问除了tcp,能不能使用http的get来进行数据交互

  • 可以的,CC3200协议支持HTTP协议,可以通过Post和Get的形式进行数据交互,可以参考CC3200-SDK的HTTP的例子进行测试。

  • Terry Han 说:

    可以的,CC3200协议支持HTTP协议,可以通过Post和Get的形式进行数据交互,可以参考CC3200-SDK的HTTP的例子进行测试。

    这个是什么情况

  • 你先用电脑尝试访问,是不是服务器那边的问题,