This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RQ:cc3100移植后调用sl_Start(0, 0, 0)死循环在_SlDrvSyncObjWaitTimeout里面

Other Parts Discussed in Thread: CC3100

cc3100移植后调用sl_Start(0, 0, 0)死循环在

retVal = _SlDrvSyncObjWaitTimeout(&g_pCB->ObjPool[ObjIdx].SyncObj,
INIT_COMPLETE_TIMEOUT,
SL_DRIVER_API_DEVICE_SL_START);

这可能是什么原因导致的?

SPI没有通?还是什么原因呢?

谢谢

  • sl_Start(0, 0, 0)是启动CC3100-NWP,CC3100的网络处理器的SP.bin文件有没有烧录到SPI Flash中?

  • T.T我们没有加SPI Flash在CC3100上。我在spi_Read 和spi_Write打断点,都没有被执行到,那sl_Start(0, 0, 0)是怎么启动CC3100-NWP的?

  • [16:39:24] Begin Format operation.
    [16:39:25] INFO: > Executing Operation: Connect
    [16:39:27] INFO: setting break signal
    [16:39:28] INFO: detecting FTDI for device reset
    [16:39:28] ERROR: No device USB ports were found
    [16:39:28] INFO: --- please restart the device ---
    [16:39:28] INFO: connection succeeded
    [16:39:28] INFO: getting storage list
    [16:39:28] INFO: > Executing Operation: Init
    [16:39:28] INFO: reading version info
    [16:39:28] INFO: DEVICE CC3100 ES1.33
    [16:39:28] INFO: reading version info
    [16:39:30] INFO: > Executing Operation: Format
    [16:39:30] INFO: Erase storage SFLASH 
    [16:39:31] INFO: erase storage succeeded
    [16:39:31] INFO: erase storage completed
    [16:39:31] INFO: > Executing Operation: Disconnect
    [16:39:31] Operation Format returned. 
    [16:39:36] Begin ServicePackProgramming operation.
    [16:39:37] INFO: > Executing Operation: Connect
    [16:39:39] INFO: setting break signal
    [16:39:40] INFO: detecting FTDI for device reset
    [16:39:40] ERROR: No device USB ports were found
    [16:39:40] INFO: --- please restart the device ---
    [16:39:43] INFO: connection succeeded
    [16:39:43] INFO: getting storage list
    [16:39:43] INFO: > Executing Operation: ServicePackProgramming
    [16:39:43] INFO: Path to the service pack file: D:/ti/CC3100_CC3200_ServicePack_1.0.1.6-2.6.0.5/servicepack_1.0.1.6-2.6.0.5.bin
    [16:39:43] INFO: reading version info
    [16:39:43] INFO: CC3100R Device detected.
    [16:39:43] INFO: NWP/MAC/PHY Version from Service Pack: 
    [16:39:43] INFO: NWP Patch version: 2.6.0.5
    [16:39:43] INFO: MAC Patch version: 1.4.0.1
    [16:39:43] INFO: PHY Patch version: 1.0.3.34
    [16:39:43] INFO: reading version info
    [16:39:43] INFO: DEVICE CC3100 ES1.33
    [16:39:43] INFO: reading version info
    [16:39:45] INFO: Downloading file "/sys/servicepack.ucf" with size 25820
    [16:39:47] INFO:

    New Token is 0x24ABEEC1
    [16:39:47] INFO: Download complete
    [16:39:47] INFO: > Executing Operation: Disconnect
    [16:39:47] Operation ServicePackProgramming returned. 
    [17:31:02] Begin Format operation.
    [17:31:02] INFO: > Executing Operation: Connect
    [17:31:04] INFO: setting break signal
    [17:31:05] INFO: connection succeeded
    [17:31:05] INFO: getting storage list
    [17:31:05] INFO: > Executing Operation: Init
    [17:31:05] INFO: reading version info
    [17:31:05] INFO: DEVICE CC3100 ES1.33
    [17:31:05] INFO: reading version info
    [17:31:07] INFO: > Executing Operation: Format
    [17:31:07] INFO: Erase storage SFLASH 
    [17:31:08] INFO: erase storage succeeded
    [17:31:08] INFO: erase storage completed
    [17:31:08] INFO: > Executing Operation: Disconnect
    [17:31:08] Operation Format returned. 
    [17:31:17] Begin ServicePackProgramming operation.
    [17:31:17] INFO: > Executing Operation: Connect
    [17:31:19] INFO: setting break signal
    [17:31:20] INFO: detecting FTDI for device reset
    [17:31:20] ERROR: No device USB ports were found
    [17:31:20] INFO: --- please restart the device ---
    [17:31:21] INFO: connection succeeded
    [17:31:21] INFO: getting storage list
    [17:31:21] INFO: > Executing Operation: ServicePackProgramming
    [17:31:21] INFO: Path to the service pack file: D:/ti/CC3100_CC3200_ServicePack_1.0.1.6-2.6.0.5/servicepack_1.0.1.6-2.6.0.5.bin
    [17:31:21] INFO: reading version info
    [17:31:21] INFO: CC3100R Device detected.
    [17:31:21] INFO: NWP/MAC/PHY Version from Service Pack: 
    [17:31:21] INFO: NWP Patch version: 2.6.0.5
    [17:31:21] INFO: MAC Patch version: 1.4.0.1
    [17:31:21] INFO: PHY Patch version: 1.0.3.34
    [17:31:21] INFO: reading version info
    [17:31:21] INFO: DEVICE CC3100 ES1.33
    [17:31:21] INFO: reading version info
    [17:31:23] INFO: Downloading file "/sys/servicepack.ucf" with size 25820
    [17:31:26] INFO:

    New Token is 0xE366105A
    [17:31:26] INFO: Download complete
    [17:31:26] INFO: > Executing Operation: Disconnect
    [17:31:26] Operation ServicePackProgramming returned.

    使用了推荐的FLASH,service pack也烧进去了,怎么程序跑到

    retVal = _SlDrvSyncObjWaitTimeout(&g_pCB->ObjPool[ObjIdx].SyncObj,
    INIT_COMPLETE_TIMEOUT,
    SL_DRIVER_API_DEVICE_SL_START);就出不来了?

    HOST_INT一直有中断。

  • SP.bin文件有没有烧录到SPI Flash中后,还是会卡在sl_Start(0, 0, 0)。测了下MCU和CC3100的MISO是没有信号的,其它的都有信号。烧后还要配置什么吗

  • 你好 你这个问题最后怎么解决的,可以分享一下吗?我和你一样的问题不知道什么原因。
  • 记不太清楚了,就是烧写对的cc3100的一个文件到FLASH就行了

  • 你好, 我也出现了类似的问题。 可以分享一下 你是怎么解决的吗?