请问TI工程师,我在用cc3100实现TCP协议,我的CC3100作server端,PC作client端。我的client端从连接状态断开后,CC3100有没有一个状态位指示已经断开了?如果有的话,这个状态位是什么?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问TI工程师,我在用cc3100实现TCP协议,我的CC3100作server端,PC作client端。我的client端从连接状态断开后,CC3100有没有一个状态位指示已经断开了?如果有的话,这个状态位是什么?谢谢!
连接断开是和AP断开连接?在回调函数中void SimpleLinkWlanEventHandler(SlWlanEvent_t *pWlanEvent) 中会有断开网络的提示信息
case SL_WLAN_DISCONNECT_EVENT:
{
slWlanConnectAsyncResponse_t* pEventData = NULL;
CLR_STATUS_BIT(g_ulStatus, STATUS_BIT_CONNECTION);
CLR_STATUS_BIT(g_ulStatus, STATUS_BIT_IP_AQUIRED);
pEventData = &pWlanEvent->EventData.STAandP2PModeDisconnected;
// If the user has initiated 'Disconnect' request,
//'reason_code' is SL_USER_INITIATED_DISCONNECTION
if(SL_USER_INITIATED_DISCONNECTION == pEventData->reason_code)
{
UART_PRINT("[WLAN EVENT]Device disconnected from the AP: %s,"
"BSSID: %x:%x:%x:%x:%x:%x on application's request \n\r",
g_ucConnectionSSID,g_ucConnectionBSSID[0],
g_ucConnectionBSSID[1],g_ucConnectionBSSID[2],
g_ucConnectionBSSID[3],g_ucConnectionBSSID[4],
g_ucConnectionBSSID[5]);
}
else
{
UART_PRINT("[WLAN ERROR]Device disconnected from the AP AP: %s,"
"BSSID: %x:%x:%x:%x:%x:%x on an ERROR..!! \n\r",
g_ucConnectionSSID,g_ucConnectionBSSID[0],
g_ucConnectionBSSID[1],g_ucConnectionBSSID[2],
g_ucConnectionBSSID[3],g_ucConnectionBSSID[4],
g_ucConnectionBSSID[5]);
}
memset(g_ucConnectionSSID,0,sizeof(g_ucConnectionSSID));
memset(g_ucConnectionBSSID,0,sizeof(g_ucConnectionBSSID));
}
break;
目前CC3100还不会将TCP FIN上传到应用层。所以需要应用层自己去探测。可以用发送数据的方式来探测。
嗯,我后面就是在发送数据或者接受数据失败的时候重新新建Socket等待连接,实现了断开后能够再次连接的功能,就是不知道这样设计合不合理。
这样可以的,需要服务器和客户端配合好。套接字在关的时候,应该会发一个TCP FIN出来的,客户端那边再重连一次就好了。