This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于cc3200的传输速率问题

Other Parts Discussed in Thread: CC3200

我看到release note里吞吐量的数据为10Mbps以上,换算为Byte应该在每秒1.5MB到2MB的样子。

我修改了http_client_demo这个例子并运行,开发板以wifi方式连接我们本地的一台AP服务器,该AP服务器上运行有一个HTTP服务器,开发板连接AP服务器后以HTTP GET方式下载一个大文件,这样测得的下载速度大概在每秒260KB到280KB之间。

请问CC3200在以WLAN client模式运行时传输速率是否就是达不到release note里标称的吞吐量,还是我的测试方法有问题?

  • 官方的测试用的如下例子和方法,不是用的http

    use the 'tcp_socket'/'udp_socket' applications of the SDK (on CC3200) with 'Iperf' (on Windows) as the other end of the socket for your throughput measurements.

    为什么不用http

    Unfortunately HTTP Throughput not available as it vary server to server. Throughput depend upon a number parameters eg. internet speed, load on server, restricted max number of request per second etc.


  • 谢谢,我跑“tcp_socket”例子,确实测到了标称值的传输速率