我想在板子的丝印P15对应的管脚输出一个高低电平信号,参考例子代码,这样写对吗:
MAP_PRCMPeripheralClkEnable(PRCM_GPIOA2,PRCM_RUN_MODE_CLK);
MAP_PinTypeGPIO(PIN_15,PIN_MODE_0, false);
MAP_GPIODirModeSet(GPIOA2_BASE,GPIO_PIN_6, GPIO_DIR_MODE_OUT);
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想在板子的丝印P15对应的管脚输出一个高低电平信号,参考例子代码,这样写对吗:
MAP_PRCMPeripheralClkEnable(PRCM_GPIOA2,PRCM_RUN_MODE_CLK);
MAP_PinTypeGPIO(PIN_15,PIN_MODE_0, false);
MAP_GPIODirModeSet(GPIOA2_BASE,GPIO_PIN_6, GPIO_DIR_MODE_OUT);
好像那个
GPIOPinWrite(GPIOA2_BASE,GPIO_PIN_6,GPIO_PIN_6);
这句有问题吧,第三个参数应该是1比较合适吧。
因为
void
GPIO_IF_Set(unsigned char ucPin,
unsigned int uiGPIOPort,
unsigned char ucGPIOPin,
unsigned char ucGPIOValue)
{
//
// Set the corresponding bit in the bitmask
//
ucGPIOValue = ucGPIOValue << (ucPin % 8);
//
// Invoke the API to set the value
//
MAP_GPIOPinWrite(uiGPIOPort,ucGPIOPin,ucGPIOValue);
}
所以知道这个函数的第4个参数就是你那个函数的第三个参数。
而例程中有:
/* Switch ON RED LED */
GPIO_IF_Set(GPIO_LED1, g_uiLED1Port, g_ucLED1Pin, 1);
break;
因此我们知道,如果输出高电平在IF SET里第4个参数是1,所以在pin WRITE函数里,第三个参数也是1.