This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200 SDK的seial_wifi例程,实时性问题

Other Parts Discussed in Thread: CC3200

TI工程你好:

        我使用的是CC3200的SDK里边的serial_wifi例程,已经能够进行正常的TCP/IP无线通信了。但是,我发现CC3200从串口写数据到wifi转发所用的时间不稳定,有的时候是几秒,有的比较快,但是整体感觉CC3200从串口开始接收数据到wifi转发这个过程大约都要几秒,请问,这个实时性问题是因为CC3200的主频80MHz的原因吗??可以改进这个实时性能吗?如何进行改进?

  • CC3200此时的RSSI值是否太小,导致信号太弱,网络信号太差?改进这个实时性能-----如果要求实时性用UDP的方式会更快,如果你的串口数据量很大,可以将串口的波特率提高,降低数据在串口本身的传输造成的固有时间差,或者直接改用SPI的方式进行数据收发,数据的吞吐量会更大

  • 你好:

            由于是和其他产品配合使用,因此必须用串口,和TCP/IP通信。至于RSSI的值的设定,我是直接用serial_wifi的样例程序,没有进行参数的修改。至于信号问题,CC3200作为AP,我用电脑连接的时候,是满格信号。我用的是板载天线,具体网络信号怎么样,怎么进行评估?

            我用的板子是淘宝上别人设计的,并不是TI的开发板,不知道你们有测试过TI开发板的serial_wifi样例程序没有?具体的数据传输速率怎么样呢??我想先知道这个大致的通信性能,进行评估后在进行开发。

    谢谢了