准备在野外测试CC3200,作为备用方案,打算用手机USB供电,有个问题:
1)PC机的usb供电的电压为5v;
2)手机USB供电的电压为3.6v;
3)CC3200硬件手册提到:外供电源3v;
那么,
1)CC3200的外供电压范围是多少?手册提到最低2.3v,最高呢?
2)能采用手机USB供电吗?
谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
准备在野外测试CC3200,作为备用方案,打算用手机USB供电,有个问题:
1)PC机的usb供电的电压为5v;
2)手机USB供电的电压为3.6v;
3)CC3200硬件手册提到:外供电源3v;
那么,
1)CC3200的外供电压范围是多少?手册提到最低2.3v,最高呢?
2)能采用手机USB供电吗?
谢谢~
1、PC机的usb供电的电压为5v
---使用PC的USB供电电源是5V,实际上是经过了CC3200Launchpad的上的降压转换芯片LDO将CC3200的实际输入电压为3.3V。
2、CC3200的外�电压范围是多少?手册提到最低2.3v,最高呢?
---通过手册中查找为最大不超过3.6,推荐典型值为3.3V
3、能采用手机USB供电吗?
---可以将手机USB供电的电压通过DCDC或者LDO的方式转换为3.3V,给CC3200供电,同时注意wifi在发射信号的瞬间电流高达200mA,要考虑你的手机USB供电
能否提供大电流瞬时输出。
在选择LDO时注意,最大输出大约在1A左右,高的动态输出响应。