This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3200电源管理问题

Other Parts Discussed in Thread: CC3200, TPS63020

版主及各位朋友,

求教一个3200的电源设计方面的问题:

我看到资料上3200有2种供电模式,1)宽范围电压供电模式  2)1.85V预稳压模式;

我的产品应用场景是3v的一次性电池供电,但电池耗尽前会慢慢降到2.2v,如果采用宽范围供电模式,cc3200的供电和正常工作没问题,但IO口电压肯定会跟随vcc的降低而下降,这样的话,我其他比如cmos sensor等都需要稳定的2.8v,1.8v供电,不可能等到电池降到低于2.8后又来升压吧,即便这样做,CC3200的IO电平和其他外围芯片也不匹配了。请教各位,有什么好的解决办法没?

如果采用1.85预稳压模式,那3200的io电平也跟随1.85v? 那外设没法对接了。1.85这个模式设计的初衷是用在什么地方呢?

多谢各位的解答!!