cc3200 smartconfig 连接wifi 很慢, 使用的是 provisioning_smartconfig 例子, 下面是串口输出的调试信息。
请教一下大家, 这是什么问题?
Host Driver Version: 1.0.0.10
Build Version 2.6.0.5.31.1.4.0.1.1.0.3.34
Device is configured in default state
Device started as STATION
[WLAN EVENT] Unexpected event [0x3] 【#define SL_WLAN_SMART_CONFIG_COMPLETE_EVENT (3)】
[WLAN EVENT] Unexpected event [0x3]
[WLAN EVENT] STA Connected to the AP: TP-LINK_836E , BSSID: e4:d3:32:90:83:6e
[NETAPP EVENT] IP Acquired: IP=192.168.1.116 , Gateway=192.168.1.1