This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3100例程tcp_socket中哪里是关于硬件的操作

Other Parts Discussed in Thread: CC3100, CC3200

我的使用模式是CC3100作为STA连到路由器,手机也连到路由器,然后CC3100和手机建立连接相互通讯,我目前想参考tcp_socket这个里面的main函数,但看了半天不知道里面是怎么跟UART或者SPI关联起来去操作硬件的,还请指教,非常感谢

  • 就是这个串口或者SPI接口接了外设,比如传感器,然后读取了数据通过TCP发送出去,是这个意思吧,cc3100应该是通过串口跟单片机通信的吧,cc3100好像是固化好的,只能使用,想控制其他外设需要其他的单片机来做。

  • CC3100是一个NWP网络处理器,负责是无线wifi网络的数据传输,需要外部配合一个单片机MCU进行UART或者SPI的通信,外部的所有外设如UART,IIC,GPIO口等都是通过外部的MCU实现的,外部的MCU采集了数据,通过UART,SPI传递给CC3100进行无线数据的发送,

    如果你想通过一个芯片实现这些内容,可以使用CC3200,这个是双核架构,一个M4内核开发给客户使用,还用一个NWP网络处理器在芯片的内部,可以进行无线数据的发送和接收。