IAR .icf文件中没有对堆栈边界及大小做划分?请问该如何配置
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
icf里有如下定义
//
// Define a block for the heap. The size should be set to something other
// than zero if things in the C library that require the heap are used.
//
define block HEAP with alignment = 8, size = 0x00008000 { };
keep {readonly section .cmdtbl};
define block CmdTbl {section .cmdtbl };
//
// Indicate that the noinit values should be left alone. This includes the
// stack, which if initialized will destroy the return address from the
// initialization code, causing the processor to branch to zero and fault.
//
do not initialize { section .noinit };
define block CSTACK with alignment = 8, size = 0x800 { section .stack };
do not initialize { section .stack};
place at end of SRAM { block CSTACK };
编译器IAR会自动进行堆栈和RAM地址的划分,你只需要修改
define block CSTACK with alignment = 8, size = 0x800 { section .stack };
do not initialize { section .stack};
place at end of SRAM { block CSTACK };
中Stack的堆栈大小值,但是注意如果堆栈修改的太大,导致你程序的RAM用量超过了分配的RAM用量就会出现问题
//
// Define a region for the on-chip flash.
//
define region FLASH = mem:[from 0x01000000 to 0x01010000];
if(CC3200_ES_1_2_1)
{
define region SRAM = mem:[from 0x20000000 to 0x20030000];
}
else
{
define region SRAM = mem:[from 0x20004000 to 0x20030000];
}