网页控制cc3200
板子在AP模式下进入网页,将其修改成sta模式,sta连上 ssid为4499的wifi上 (重启之后生效这个过程应该怎么制作出来?)
将其设置为sta 设置连接到4499的wifi上 重启之后怎么让他自动连接到4499的wifi上呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
网页控制cc3200
板子在AP模式下进入网页,将其修改成sta模式,sta连上 ssid为4499的wifi上 (重启之后生效这个过程应该怎么制作出来?)
将其设置为sta 设置连接到4499的wifi上 重启之后怎么让他自动连接到4499的wifi上呢?
我在网页上修改AP的名称和密码 我想重启后 AP设置为我网页上修改的那个
我应该怎么做呢?
重启后好像只有AP名称是上一次ap的 密码直接为open
我想重启后直接为上次ap的配置 包括密码
CC3200在连接到AP后保存Profile,在CC3200再次启动后,注意不要将所有的Profile删除,否则就无法连接到你之前记录的路由器AP上了,在程序中查找
//*****************************************************************************
//! \brief This function puts the device in its default state. It:
//! - Set the mode to STATION
//! - Configures connection policy to Auto and AutoSmartConfig
//! - Deletes all the stored profiles -----------------------------------------------------------这个地方不要打开,否则会删除所有的Profile
//! - Enables DHCP
//! - Disables Scan policy
//! - Sets Tx power to maximum
//! - Sets power policy to normal
//! - Unregister mDNS services
//! - Remove all filters
//!
//! \param none
//! \return On success, zero is returned. On error, negative is returned
//*****************************************************************************
static long ConfigureSimpleLinkToDefaultState()
SlVersionFull ver = {0};
_WlanRxFilterOperationCommandBuff_t RxFilterIdMask = {0};
unsigned char ucVal = 1;
unsigned char ucConfigOpt = 0;
unsigned char ucConfigLen = 0;
unsigned char ucPower = 0;
long lRetVal = -1;
long lMode = -1;
lMode = sl_Start(0, 0, 0);
ASSERT_ON_ERROR(lMode);
// If the device is not in station-mode, try configuring it in station-mode
if (ROLE_STA != lMode)
{
if (ROLE_AP == lMode)
{
// If the device is in AP mode, we need to wait for this event
// before doing anything
while(!IS_IP_ACQUIRED(g_ulStatus))
{
#ifndef SL_PLATFORM_MULTI_THREADED
_SlNonOsMainLoopTask();
#endif
}
}
// Switch to STA role and restart
lRetVal = sl_WlanSetMode(ROLE_STA);
ASSERT_ON_ERROR(lRetVal);
lRetVal = sl_Stop(0xFF);
ASSERT_ON_ERROR(lRetVal);
lRetVal = sl_Start(0, 0, 0);
ASSERT_ON_ERROR(lRetVal);
// Check if the device is in station again
if (ROLE_STA != lRetVal)
{
// We don't want to proceed if the device is not coming up in STA-mode
return DEVICE_NOT_IN_STATION_MODE;
}
}
// Get the device's version-information
ucConfigOpt = SL_DEVICE_GENERAL_VERSION;
ucConfigLen = sizeof(ver);
lRetVal = sl_DevGet(SL_DEVICE_GENERAL_CONFIGURATION, &ucConfigOpt,
&ucConfigLen, (unsigned char *)(&ver));
ASSERT_ON_ERROR(lRetVal);
UART_PRINT("Host Driver Version: %s\n\r",SL_DRIVER_VERSION);
UART_PRINT("Build Version %d.%d.%d.%d.31.%d.%d.%d.%d.%d.%d.%d.%d\n\r",
ver.NwpVersion[0],ver.NwpVersion[1],ver.NwpVersion[2],ver.NwpVersion[3],
ver.ChipFwAndPhyVersion.FwVersion[0],ver.ChipFwAndPhyVersion.FwVersion[1],
ver.ChipFwAndPhyVersion.FwVersion[2],ver.ChipFwAndPhyVersion.FwVersion[3],
ver.ChipFwAndPhyVersion.PhyVersion[0],ver.ChipFwAndPhyVersion.PhyVersion[1],
ver.ChipFwAndPhyVersion.PhyVersion[2],ver.ChipFwAndPhyVersion.PhyVersion[3]);
// Set connection policy to Auto + SmartConfig
// (Device's default connection policy)
lRetVal = sl_WlanPolicySet(SL_POLICY_CONNECTION,
SL_CONNECTION_POLICY(1, 0, 0, 0, 1), NULL, 0);
ASSERT_ON_ERROR(lRetVal);
// Remove all profiles
lRetVal = sl_WlanProfileDel(0xFF);------------------------------------------------------------------不要删除所有的Profile
ASSERT_ON_ERROR(lRetVal);
//
// Device in station-mode. Disconnect previous connection if any
// The function returns 0 if 'Disconnected done', negative number if already
// disconnected Wait for 'disconnection' event if 0 is returned, Ignore
// other return-codes
//
lRetVal = sl_WlanDisconnect(); //会把标志位置位,中断是在后面发生的!在后面清除标志位
if(0 == lRetVal)
{
// Wait
while(IS_CONNECTED(g_ulStatus))
{
#ifndef SL_PLATFORM_MULTI_THREADED
_SlNonOsMainLoopTask();
#endif
}
}
// Enable DHCP client
lRetVal = sl_NetCfgSet(SL_IPV4_STA_P2P_CL_DHCP_ENABLE,1,1,&ucVal);
ASSERT_ON_ERROR(lRetVal);
// Disable scan
ucConfigOpt = SL_SCAN_POLICY(0);
lRetVal = sl_WlanPolicySet(SL_POLICY_SCAN , ucConfigOpt, NULL, 0);
ASSERT_ON_ERROR(lRetVal);
// Set Tx power level for station mode
// Number between 0-15, as dB offset from max power - 0 will set max power
ucPower = 0;
lRetVal = sl_WlanSet(SL_WLAN_CFG_GENERAL_PARAM_ID,
WLAN_GENERAL_PARAM_OPT_STA_TX_POWER, 1, (unsigned char *)&ucPower);
ASSERT_ON_ERROR(lRetVal);
//add
//lRetVal = sl_WlanPolicySet(SL_POLICY_CONNECTION , SL_CONNECTION_POLICY(1,1,0,0,0), 0, 0);
// Set PM policy to normal
lRetVal = sl_WlanPolicySet(SL_POLICY_PM , SL_NORMAL_POLICY, NULL, 0);
ASSERT_ON_ERROR(lRetVal);
// Unregister mDNS services
lRetVal = sl_NetAppMDNSUnRegisterService(0, 0);
ASSERT_ON_ERROR(lRetVal);
// Remove all 64 filters (8*8)
memset(RxFilterIdMask.FilterIdMask, 0xFF, 8);
lRetVal = sl_WlanRxFilterSet(SL_REMOVE_RX_FILTER, (_u8 *)&RxFilterIdMask,
sizeof(_WlanRxFilterOperationCommandBuff_t));
ASSERT_ON_ERROR(lRetVal);
lRetVal = sl_Stop(SL_STOP_TIMEOUT);
ASSERT_ON_ERROR(lRetVal);
InitializeAppVariables();
return lRetVal; // Success
}