本来对WIFI就不太理解,TI提供的例程又是操作系统下使用的,对它的过程调用就很难看了。手里的CC3200板子总想捣鼓一下,苦于没有适当的例程参考。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有没有操作系统的例子,参考cc3200-sdk\example\tcp_socket中的例子,有很多都是没有操作系统的
void main()
{
long lRetVal = -1;
//
// Board Initialization
//
BoardInit();
//
// Initialize the uDMA
//
UDMAInit();
//
// Configure the pinmux settings for the peripherals exercised
//
PinMuxConfig();
//
// Configuring UART
//
InitTerm();
//
// Display banner
//
DisplayBanner(APPLICATION_NAME);
InitializeAppVariables();
//---------------------------并未加入(2) 启动SimpleLink Host-------------------------
//
// Start the SimpleLink Host
//
// lRetVal = VStartSimpleLinkSpawnTask(SPAWN_TASK_PRIORITY);
// if(lRetVal < 0)
// {
// ERR_PRINT(lRetVal);
// LOOP_FOREVER();
// }
//-----------------------------------------------------------------------
//
// Following function configure the device to default state by cleaning
// the persistent settings stored in NVMEM (viz. connection profiles &
// policies, power policy etc)
//
// Applications may choose to skip this step if the developer is sure
// that the device is in its default state at start of applicaton
//
// Note that all profiles and persistent settings that were done on the
// device will be lost
//
lRetVal = ConfigureSimpleLinkToDefaultState();
if(lRetVal < 0)
{
if (DEVICE_NOT_IN_STATION_MODE == lRetVal)
UART_PRINT("Failed to configure the device in its default state \n\r");
LOOP_FOREVER();
}
UART_PRINT("Device is configured in default state \n\r");
//
// Asumption is that the device is configured in station mode already
// and it is in its default state
//
lRetVal = sl_Start(0, 0, 0);
if (lRetVal < 0)
{
UART_PRINT("Failed to start the device \n\r");
LOOP_FOREVER();
}
UART_PRINT("Device started as STATION \n\r");
UART_PRINT("Connecting to AP: %s ...\r\n",SSID_NAME);
// Connecting to WLAN AP - Set with static parameters defined at common.h
// After this call we will be connected and have IP address
lRetVal = WlanConnect();
if(lRetVal < 0)
{
UART_PRINT("Connection to AP failed \n\r");
LOOP_FOREVER();
}
UART_PRINT("Connected to AP: %s \n\r",SSID_NAME);
UART_PRINT("Device IP: %d.%d.%d.%d\n\r\n\r",
SL_IPV4_BYTE(g_ulIpAddr,3),
SL_IPV4_BYTE(g_ulIpAddr,2),
SL_IPV4_BYTE(g_ulIpAddr,1),
SL_IPV4_BYTE(g_ulIpAddr,0));
#ifdef USER_INPUT_ENABLE //定义了USER_INPUT_ENABLE
lRetVal = UserInput();
if(lRetVal < 0)
{
ERR_PRINT(lRetVal);
LOOP_FOREVER();
}
#else //不执行
lRetVal = BsdTcpClient(PORT_NUM); //建立CC3200-TCP Client并向目的IP及端口号5001发送TCP数据
if(lRetVal < 0)
{
UART_PRINT("TCP Client failed\n\r");
LOOP_FOREVER();
}
lRetVal = BsdTcpServer(PORT_NUM); //建立TCP Server 等待连接并接收数据
if(lRetVal < 0)
{
UART_PRINT("TCP Server failed\n\r");
LOOP_FOREVER();
}
#endif
UART_PRINT("Exiting Application ...\n\r");
//
// power of the Network processor
//
lRetVal = sl_Stop(SL_STOP_TIMEOUT);
while (1)
{
_SlNonOsMainLoopTask();
}
}
您可以参考TI wiki页面的说明 http://processors.wiki.ti.com/index.php/CC32xx_SDK_Sample_Applications
很多都是Non-OS的