TI工程师以及各位伙伴你们好,我现在项目中需要同时用到CC3200的串口0以及串口一,串口一想把PIN57/58配置成串口一的收发,但是一直不太明白评估版上VCC与PIN58引脚通过跳线帽连接是为什么???请各位多多指教
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI工程师以及各位伙伴你们好,我现在项目中需要同时用到CC3200的串口0以及串口一,串口一想把PIN57/58配置成串口一的收发,但是一直不太明白评估版上VCC与PIN58引脚通过跳线帽连接是为什么???请各位多多指教
注意在CC3200的Launchpad中关于UART0的引脚需要
注意必须将J6跳线帽连接才能将该引脚分配到LP外扩的PIN脚,同时注意不要使用UART0-RX该脚接了按键10k电阻到地,在UART0_RX中必须将跳线帽连接才能将该引脚分配到LP外扩的PIN脚!
PIN58直接通过跳线帽与VCC连接的目的是在Out of box 例程中,通过Pin58引脚读取高电平来选择CC3200作为AP/Station 模式,如果你想使用UART1直接将PIN58的上拉跳线帽拔掉,然后通过Pin MUX工具选择UART1的功能引脚,生成对应的引脚.c和.h函数添加到CC3200的工程中即可以使用UART1具体的引脚了。