TI 工程师,你好:
我使用 File Download demo的时候,出现了 -2009错误,有知道是什么原因?
CC3200 File Download Application
*************************************************
Host Driver Version: 1.0.1.6
Build Version 2.7.0.0.31.1.4.0.1.1.0.3.34
Device is configured in default state
Device started as STATION
[WLAN EVENT] STA Connected to the AP: NxecoI , BSSID: bc:d1:77:8:b1:4b
[NETAPP EVENT] IP Acquired: IP=192.168.1.9 , Gateway=192.168.1.1
Connected to the AP: NxecoI
Connection to server created successfully
Start downloading the file
Content length: 90826
Failed during writing the file, Error-code: -2009
Downloading File Completed
Thank you