OOB例程 实现不了所说的功能?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC3200的原始程序是SDK中的例程
C:\ti\CC3200SDK_1.2.0\cc3200-sdk\example\out_of_box
详细的资料参考CC32xx Out of Box Application.pdf
CC32xx Out of Box Application
Overview
This Application demonstrates Out of Box Experience with CC3200
Launch Pad. It highlights the following features
1. Easy Connection to CC3200 Launchpad
• Direct Connection to Launchpad by using CC3200 device in
Access Point Mode(Default)
• Connection using TI SmartConfig [1]Technology
2. Easy access to CC3200 Using Internal HTTP server and on-board webcontent
3. Attractive Demos
• Home Automation
• Appliance Control
• Security System
• Thermostat
For more information please refer CC32xx Quick Start Guide
Usage
• The CC3200 Launchpad comes with all the required content flashed to run the application
• Refer Quick Start Guide for detailed information
• In case user flashed other SDK applications and need to download the out of box content again, follow below
steps
• Open <cc3200-sdk>\examples\out_of_box\html\out_of_box.ucf session file in Uniflash.
• Flash the files to the device. Detailed instructions at Uniflash User Guide.
• Run the reference application
1. Run From IDE (IAR/CCS)
• Open the Example Project as mentioned in the <cc3200-sdk>\docs\CC3200-Getting Started Guide.pdf
• Build and download the application to the board
2. Run From Flashed Binary
• Connect to CC3200 device as mentioned in Quick Start Guide, You will see below main page on your browser
Note: : In case device is coming up as AP (Jumper on VCC+P58) check Terminal prints to get to know device's AP
name.