This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
让CC3200进入hibernate的方式通过调用指令:
void EnterHIBernate()
{
#define SLOW_CLK_FREQ (32*1024)
//
// Configure the HIB module RTC wake time
//
MAP_PRCMHibernateIntervalSet(5 * SLOW_CLK_FREQ);
//
// Enable the HIB RTC
//
// MAP_PRCMHibernateWakeupSourceEnable(PRCM_HIB_SLOW_CLK_CTR);
//------------------------------------------------------------Hib模式下增加GPIO唤醒---------------------------------------------------------------
// PRCMHibernateWakeupSourceEnable入口参数
// PRCM_HIB_SLOW_CLK_CTR -PRCM_HIB_GPIO2 -PRCM_HIB_GPIO4 -PRCM_HIB_GPIO13 -PRCM_HIB_GPIO17 -PRCM_HIB_GPIO11 -PRCM_HIB_GPIO24 -PRCM_HIB_GPIO26
PRCMHibernateWakeupSourceEnable(PRCM_HIB_GPIO13);
PRCMHibernateWakeUpGPIOSelect(PRCM_HIB_GPIO13,PRCM_HIB_FALL_EDGE); //按键按下去产生上升沿,松开后产生下降沿!注意入口参数的顺序!!!
//------------------------------------------------------------------------------------------------------------------------------------------------
// DBG_PRINT("HIB: Entering HIBernate...\n\r");
UART_PRINT("Entering HIB\n\r");
MAP_UtilsDelay(80000);
//
// powering down SPI Flash to save power
//
Utils_SpiFlashDeepPowerDown();
//
// Enter HIBernate mode
//
MAP_PRCMHibernateEnter();
}
CC3200从Hibernate唤醒的时间:
Wake-up time is longer than LPDS mode at about 15 ms plus the time to load the application from serial flash, which varies according to code size.
实验室实际测试功耗记录(测试代码 idle_profile_nonos): 模式 条件 电流消耗 测试图 Datasheet
M4 Active(80MHz)+NWP connect AP 1 15.9mA 图 1 15.3mA
M4 LPDS+NWP start but do nothing 2 282uA 图 2 266uA
M4 LPDS+NWP connect AP<1> 3 600uA~2mA(Avr=900uA) 图 3 图 4 825uA
M4 LPDS+NWP Hib<2> 4 229uA 图 5 120uA
M4 Hib+NWP Hib 5 10.65uA 图 6 4uA 备注: M4 LPDS(RAM-Retained)/Hib(RAM-Not Retained) 唤醒: RTC+GPIO(UART 复用 GPIO)
M4 Active+NWP connect AP =15.9mA
M4 LPDS+NWP connect AP =600uA~2mA 波动 大约平均功耗为 1mA 左右
M4 LPDS+NWP start but do nothing 即 sl_start 但不连接 AP =282uA
M4 LPDS+NWP 进入 Hib 模式 229uA 注意此时网络已经断开,但是 RAM 还是保存的!
M4 Hib+NWP 进入 Hib 模式 10.65uA(注意 Hib 模式下测试的电流消耗为 CC3200+SPI_Flash 的功耗,而 Datasheet 上 4uA 是不包括 SPI_Flash 的功耗)