This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于cc3200的市场应用

Other Parts Discussed in Thread: CC3200, CC3220S, CC3220R, CC3220SF

笔者接触3200有两年的时间了,目前应用在两款网关上,一个本地网关一个86盒网关。可以说3200问题是不少的,而且有些还是致命的问题,但是我还是用在了量产产品上,因为我在实验室放了五个月没有一次离线。下一步要规划个无线视频传输的方案,估计还是用3200做了。

我有个疑问,目前市面上使用3200的产品是少之又少的,大家都有什么量产的使用了这款芯片了?目前大家都是单向的跟TI的技术人员交流,这种信息太少了。

  • 建议参考CC3200的升级芯片CC3220,该芯片有内置1M的Flash,还有安全性的加入,已经硬件RF中的Smartcofig兼用性大幅改进,

    http://www.ti.com.cn/product/cn/CC3220?keyMatch=CC3220&tisearch=Search-CN-Everything

    • CC3220x SimpleLink™ Wi-Fi® Wireless Microcontroller Unit (MCU) System-on-Chip (SoC) is a Single-Chip With Two Separate Execution Environments: a User Application Dedicated ARM® Cortex®-M4 MCU and a Network Processor MCU to Run All Wi-Fi and Internet Logical Layers
    • Chip-Level, Wi-Fi Alliance Wi-Fi CERTIFIED
    • Applications Microcontroller Subsystem
      • ARM Cortex-M4 Core at 80 MHz
      • Embedded Memory
        • The CC3220R and CC3220S Variants Include 256KB of RAM
        • The CC3220SF Variant is a Flash-Based Wireless MCU With Integrated 1MB of Flash and 256KB of RAM
        • External Serial Flash
      • McASP Supports Two I2S Channels
      • SD
      • SPI
      • I2C
      • UART
      • 8-Bit Parallel Camera
      • Four General-Purpose Timers With 16-Bit PWM Mode
      • Watchdog Timer
      • 4-Channel 12-Bit ADCs
      • Up to 27 GPIO Pins
      • Debug Interfaces: JTAG, cJTAG, SWD
    • Wi-Fi Network Processor (NWP) Subsystem
      • Wi-Fi Internet-on-a-chip Dedicated ARM MCU Completely Offloads Wi-Fi and Internet Protocols from the Application MCU
      • Wi-Fi Modes:
        • 802.11b/g/n Station
        • 802.11b/g Access Point (AP) Supports up to Four Stations
        • Wi-Fi Direct Client and Group Owner
      • WPA2 Personal and Enterprise Security: WEP, WPA/WPA2 PSK, WPA2 Enterprise (802.1x)
      • IPv4 and IPv6 TCP/IP Stack
      • Industry-Standard BSD Socket Application Programming Interfaces (APIs)
        • 16 Simultaneous TCP or UDP Sockets
        • 6 Simultaneous TLS and SSL Sockets
      • IP Addressing: Static IP, LLA, DHCPv4, DHCPv6 With DAD

  • 我只问一个问题,这个升级版的能把双频的一键配置问题解决吗?