This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc3200与路由器连接不稳定

Other Parts Discussed in Thread: CC3200

TI工程师你们好!

        在使用cc3200芯片的时候,在程序中已经实现了已与路由器连接可以上网。使用freertos系统、TCP方式与外部30s进行一次心跳通信,但是发现1、有时候TCP发送数据的时候,频繁的sl_Send()函数的返回值是-1。2、在有些路由器上面,网络是稳定的,但是有些路由器上面出现网络老是掉线的问题,但是手机端的话几乎没有这个问题。针对问题1与2,麻烦给出一些建议

  • 看看是不是有些路由器支持的频道有关。

  • 这个跟cc3200有什么关系呢?或者如何解决这个问题呢!确保cc3200与路由器在一个频道呢

  • 安卓手机可以用WiFi Analysis软件查看路由器启动后的WiFi信道,可以调节路由器的信道在任意1~12中,目的是避开环境中拥堵的信道,这时CC3200启动后就会自动的连接到指定路由器下的相对干净的信道中,保证连接的稳定性和传输的稳定性。

  • 1.意思是不是说,通过手机端的设置,改变路由器的信道在一个比较良好的信道,然后cc3200在连接到路由器上之后就会有一个相对稳定的网络环境?

    2.在使用过程中,发现有些路由器手机端连接是稳定的,但是cc3200连接的时候有时候会频繁断网,遇见这种情况下,硬件端应该如何处理来保证网络与手机端一样稳定呢?

  • 1、理解的非常正确,通过改变路由器的信道,可以让CC3200在连接该路由器后获得一个相对较为干净的网络

    2、手机连接稳定可能是手机的发射功率及接收灵敏度相对较高,如果你是自己设计的CC3200板卡,建议对天线的射频参数做好匹配,将接收灵敏度调制最优的效果,这样就会保证在连接的过程中不会出现频繁断网的现象。