This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于3200的改进建议和需求

Other Parts Discussed in Thread: CC3200, CC3220S, CC3220R, CC3220SF

两个问题:

1、cc3200有没有计划推出后续的改进型号?

2、我们做医疗植入式产品,想产品化开发的话需要3200有一些改进,比如缩小尺寸、更集成的电源管理等,这些具体的改进需求我们可以整理成文档,想请问你们TI有没有一个渠道或部门能够跟我们探讨这些问题,或者说专门负责搜集行业用户的需求,甚至谈一些合作。

  • 1. CC3200的升级芯片已经发布并量产,详细链接

    http://www.ti.com/product/CC3220?keyMatch=CC3220&tisearch=Search-EN-Everything

    • CC3220x SimpleLink™ Wi-Fi® Wireless Microcontroller Unit (MCU) System-on-Chip (SoC) is a Single-Chip With Two Separate Execution Environments: a User Application Dedicated ARM® Cortex®-M4 MCU and a Network Processor MCU to Run All Wi-Fi and Internet Logical Layers
    • Chip-Level, Wi-Fi Alliance Wi-Fi CERTIFIED
    • Applications Microcontroller Subsystem
      • ARM Cortex-M4 Core at 80 MHz
      • Embedded Memory
        • The CC3220R and CC3220S Variants Include 256KB of RAM
        • The CC3220SF Variant is a Flash-Based Wireless MCU With Integrated 1MB of Flash and 256KB of RAM
        • External Serial Flash
      • McASP Supports Two I2S Channels
      • SD
      • SPI
      • I2C
      • UART
      • 8-Bit Parallel Camera
      • Four General-Purpose Timers With 16-Bit PWM Mode
      • Watchdog Timer
      • 4-Channel 12-Bit ADCs
      • Up to 27 GPIO Pins
      • Debug Interfaces: JTAG, cJTAG, SWD
    • Wi-Fi Network Processor (NWP) Subsystem
      • Wi-Fi Internet-on-a-chip Dedicated ARM MCU Completely Offloads Wi-Fi and Internet Protocols from the Application MCU
      • Wi-Fi Modes:
        • 802.11b/g/n Station
        • 802.11b/g Access Point (AP) Supports up to Four Stations
        • Wi-Fi Direct Client and Group Owner
      • WPA2 Personal and Enterprise Security: WEP, WPA/WPA2 PSK, WPA2 Enterprise (802.1x)
      • IPv4 and IPv6 TCP/IP Stack
      • Industry-Standard BSD Socket Application Programming Interfaces (APIs)
        • 16 Simultaneous TCP or UDP Sockets
        • 6 Simultaneous TLS and SSL Sockets
      • IP Addressing: Static IP, LLA, DHCPv4, DHCPv6 With DAD
      • SimpleLink Connection Manager for Autonomous and Fast Wi-Fi Connections
      • Flexible Wi-Fi Provisioning With SmartConfig Technology, AP Mode, and WPS2 Options
      • RESTful API Support Using the Internal HTTP Server
      • Embedded Network Applications Running on Dedicated Network Processor

    More Information

    • The CC3220 device family offers three variations. Please see data sheet for more information
      • Pin to pin compatible
      • 1MB flash
      • 256kB of RAM
      • Enhanced application level security
  • 关键是第二个问题,也麻烦确认一下。