This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于cc3200应用的2个问题

Other Parts Discussed in Thread: CC3200

RT,由于我们的应用场景为cc3200后端直接对接相应的PC端服务器,

CC3200先通过STA模式接入服务器所局域网的路由器,路由器通过有线方式与服务器连接。

问题:

           1.如果我们需要在这种环境下面实现cc3200demo中的mDNS功能(即cc3200上电后直接运行mDNS线程与PC端(windos 7)相关的mDNS客户端建立连接并通信),请问cc3200 mDNS功能有windows 环境下面的例程吗?

           2.如果我们需要在PC端实现 cc3200上的 smartconfig功能,请问PC端有相应的例程吗?

  • 1. mDNS可以参考SDK的例程

    \cc3200-sdk\example\mdns

    2. http://www.ti.com/tool/smartconfig?keyMatch=smartconfig&tisearch=Search-EN-Everything

  • 建议采用AP 方式代替smartconfig. smartconfig不是100%成功的。

    http://processors.wiki.ti.com/index.php/CC32xx_Provisioning_AP

    CC32xx Provisioning AP

    Cc31xx cc32xx return home.png
    Cc32xx return sample apps.png

    Overview and Application details

    This user guide describes all the steps needed to use this example, in which the CC3200 device is used in conjunction with a Wi-Fi enabled mobile device running an application (in this case Simplelink Wi-Fi Starter Pro) and allowing it to connect to the Wi-Fi network.

    NoteNote: This wiki page is only applicable for CC3200-SDK v1.2.0 and upward releases. For documentation on older SDKs' examples, refer corresponding file in<cc3200-sdk-installation-location>\cc3200-sdk\docs\examples\

    The TI SimpleLink Starter Pro application can be downloaded from the App Store (iOS) or Google play (Android).

    NoteNote: There are two versions of the SimpleLink Wi-Fi starter applications on the Play Store. Please make sure to choose the “Pro” version.

    Prerequisites

    Setup Environment

    Provisioning set up is illustrated in the picture below. It consists of the SimpleLink Wi-Fi device being provisioned, a smart phone (Android or iPhone) with TI SimpleLink Starter Pro Application installed and an access point/router (for connection to the Internet).

    Provisioning high level view.png

    Usage

    • Connect the board to a Windows-PC and configure the terminal-program for seeing the logs - CC31xx & CC32xx Terminal Setting has detailed instructions for configuring the terminal-program. Please refer CC3200 Getting started Guide for terminal connection. This provisioning application, works only with SDK1.2
    • Install the 'provisioning add-on package' to the SDK1.2. The 'add-on' installs, provisioning library and the provisioning application. (The below pictures show the installation for CC3200 SDK).

    Cc3200 provisioning addon lib location.png

    Cc3200 provisioning addon example location.png

    • Open CCS workspace, import the provisioning library and application as illustrated below.

    Cc3200 provisioning addon ccs import.png

    • Build provisioning library, followed by the provisioning application:

    Cc3200 provisioning addon projects.png

    • After the application is built, either flash or load the application from CCS and run. The application configures the device in SimpleLink Provision mode. The device will then wait for the SimpleLink Starter Pro application to provision it to a Wi-Fi network.
    • Run TI SimpleLink Starter Pro Application on your Smartphone

    Cc3100 cc3200 simplelink provisioning app 01.png

    • Configuration page pops up, on the smart phone. Select the drop-down menu for ‘Device to configure’ and select the SimpleLink device to configure.

    Cc3100 cc3200 simplelink provisioning app 02.png Cc3100 cc3200 simplelink provisioning app 03.png Cc3100 cc3200 simplelink provisioning app 04.png

    By default, the page displays all the access points with the name beginning with "mysimplelink-". If the device to be provisioned is named differently, select "Show all", which shows all the access points in the vicinity. And, now select the SimpleLink device to be provisioned. This takes us back to the Configuration page.

    • The next step is to select/configure the Wi-Fi network and optionally name the device. Select the drop-down menu ‘Wi-Fi network’.

    Cc3100 cc3200 simplelink provisioning app 05.png Cc3100 cc3200 simplelink provisioning app 06.png

    If the pop-up page does not show all the Wi-Fi routers, select ‘Show all’, this makes the SimpleLink Wi-Fi device, to send the complete scan list to the phone app.

    Cc3100 cc3200 simplelink provisioning app 07.png Cc3100 cc3200 simplelink provisioning app 08.png

    Select the Wi-Fi router and enter the Wi-Fi network authentication type and password. Press 'Start Configuration' button to start the provisioning process. Several status messages are displayed on the screen, as the provisioning process continues.

    Cc3100 cc3200 simplelink provisioning app 09.png Cc3100 cc3200 simplelink provisioning app 10.png

    • If provisioning has succeeded, ‘Provisioning Successful’ shows up.

    Cc3100 cc3200 simplelink provisioning app 11.png

    • In the event of failure, please check the following:

    Cc3100 cc3200 simplelink provisioning app 12.png

    1. Ensure that the password and SSID entered for the access point are correct.
    2. The SimpleLink device is in Provisioning mode.
    3. The phone (with the running provisioning app) and the device are within the AP range.
    4. Check the console for error messages, and send the error logs using the phone app.

    Cc3100 cc3200 simplelink provisioning app 13.png Cc3100 cc3200 simplelink provisioning app 14.png Cc3100 cc3200 simplelink provisioning app 15.png

    In the event of failure, try couple of time by Resetting the device (For 'Reset' button location, please refer to the CC3200 Quick Start Guide)

    • On success, user can check that the device is listed in the ‘Devices’ page of the phone application and connect to it.

    Cc3100 cc3200 simplelink provisioning app 16.png Cc3100 cc3200 simplelink provisioning app 17.png Cc3100 cc3200 simplelink provisioning app 18.png

    • See the logs on the terminal-program's console. On success, below message will be displayed on the terminal

    Cc3200 simplelink provisioning console sample.png

    Limitations/Known Issues

    None