This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教关于开发板连mPCI-e接口的WiFi模块的问题

Other Parts Discussed in Thread: AM5726

我在am5726开发板上接了一个mPCI-e接口的WiFi卡(Intel ac3160的)在dmesg | grep wifi 出现L1 disable - LTR disable

ifconfig wlp1s0(WiFi网卡名) up 也是显示

iwlwifi 0000:01:00.0: L1 disable - LTR disable

iwlwifi 0000:01:00.0: L1 disable - LTR disable

iwlwifi 0000:01:00.0: Failed to load firmware chunk!

iwlwifi 0000:01:00.0: Could not load the [0] uCode section

iwlwifi 0000:01:00.0: Failed to start INIT ucode: -110

iwlwifi 0000:01:00.0: Failed to run INIT ucode: -110

请教一下这是WiFi卡硬件的问题还是内核配置问题,如果是配置问题,还需要配置什么?谢谢