请问 CC3200 的 无线wifi数据传输带宽有多大?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
|
STA Mode |
|||
|
|
SL Studio |
CC3200 |
|
|
Security |
Traffic |
SPI 15MHz |
SPI 20MHz |
|
Open |
UDP Tx |
12.7Mbps |
15.9Mbps |
|
UDP Rx |
10.5Mbps |
16.1Mbps |
|
|
TCP Tx |
12.8Mbps |
16.2Mbps |
|
|
TCP Rx |
11.3Mbps |
15.3Mbps |
|
|
TLS |
TCP Tx |
12.8Mbps |
12.4Mbps |
|
TCP Rx |
11.1Mbps |
11.8Mbps |
|
|
SSL |
TCP Tx |
8.8Mbps |
8.5Mbps |
|
TCP Rx |
9.8Mbps |
9.8 Mbps |
|
|
AP Mode |
|||
|
|
SL Studio |
CC3200 |
|
|
Security |
Traffic |
SPI 15MHz |
SPI 20MHz |
|
Open |
UDP Tx |
12.9Mbps |
16.0Mbps |
|
UDP Rx |
10.5Mbps |
16.1Mbps |
|
|
TCP Tx |
12.9Mbps |
16.4Mbps |
|
|
TCP Rx |
11.3Mbps |
15.1Mbps |
|
|
TLS |
TCP Tx |
12.5Mbps |
12.0Mbps |
|
TCP Rx |
11.3Mbps |
11.6Mbps |
|
|
SSL |
TCP Tx |
8.4Mbps |
8.1Mbps |
|
TCP Rx |
9.6Mbps |
9.9Mbps |
|
TI 无线WiFi还有WL 系列wifi 处理性能更强
http://www.ti.com/product/WL1837MOD/datasheet/detailed_description?keyMatch=WL18&tisearch=Search-EN-Everything