如题,有这方面的需求,希望可以解答一下。
如果有例程可以参考是最好的了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果需要SPI传输大量的数据建议使用DMA的模式,
可以参考udma和UART-dma的例子,主要是弄清楚dma的使用方法,可以参考SPI-DMA的例子,
可以参考一个SPI DMA的例子,
https://github.com/severin-kacianka/cc3200_dma_spi_example/
Here are two examples that show how to use SPI with DMA and FIFO on the CC3200. I hope that they are a useful starting point for anyone, who wants to work on SPI and DMA in the future.
The examples are compiling fine on Linux with gcc 4.9.3 from http://launchpad.net/gcc-arm-embedded. All you need to change is the path for the SDK in the Makefile. The hardware setup is similar to the SPI example in the SDK: just connect two CC3200 via cable (Pins GND, P05, P06, P07 and P08). I have set the following jumpers: J6, J7, J8. J9. J10, J11, J12, J13.
simple_spi_transfer is an example of an SPI transfer without DMA and FIFO. The master sends a buffer to the slave, reads it back in the next transfers and verifies the checksums.
transfer_1024_byte implements a simple SPI/DMA transfer that will transfer 1024 (or whatever DMA_SIZE is set to) bytes from the master to the slave and back. It then calculates the buffer's CRC checksum and (on the master) compares the send checksum to the received checksum.
transfer_64k shows how to transfer a 64k buffer from the master to the slave and back again.
windows contains a Makefile send to me by Matt van de Werken that also works using the Launchpad tools in a Cygwin enviroment