This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200 SPI通信做从机 STA模式WIFI通信

Other Parts Discussed in Thread: CC3200

请问,我想把CC3200作为STA模式与服务器进行无线连接。并把CC3200作为SPI的从机,与外部SPI的主机进行数据的传输。串口实现的例程我有了解过,但是SPI实现这个功能还是一头雾水,有这方面的例程吗。求指导,谢谢。

  • 如果需要SPI传输大量的数据建议使用DMA的模式,

    可以参考一个SPI DMA的例子,

    https://github.com/severin-kacianka/cc3200_dma_spi_example/

    cc3200_dma_spi_example

    Here are two examples that show how to use SPI with DMA and FIFO on the CC3200. I hope that they are a useful starting point for anyone, who wants to work on SPI and DMA in the future.

    The examples are compiling fine on Linux with gcc 4.9.3 from http://launchpad.net/gcc-arm-embedded. All you need to change is the path for the SDK in the Makefile. The hardware setup is similar to the SPI example in the SDK: just connect two CC3200 via cable (Pins GND, P05, P06, P07 and P08). I have set the following jumpers: J6, J7, J8. J9. J10, J11, J12, J13.

    simple_spi_transfer is an example of an SPI transfer without DMA and FIFO. The master sends a buffer to the slave, reads it back in the next transfers and verifies the checksums.

    transfer_1024_byte implements a simple SPI/DMA transfer that will transfer 1024 (or whatever DMA_SIZE is set to) bytes from the master to the slave and back. It then calculates the buffer's CRC checksum and (on the master) compares the send checksum to the received checksum.

    transfer_64k shows how to transfer a 64k buffer from the master to the slave and back again.

    windows contains a Makefile send to me by Matt van de Werken that also works using the Launchpad tools in a Cygwin enviroment