程序是自己参考timer demo写的,经过UART调试发现,定时器中断没有进入,对比了timer demo,也没发现错误,请问问题出在哪里?以下是代码:
/*
* main.c
*/
#include"hw_types.h"
#include"hw_memmap.h"
#include"hw_ints.h"
#include"rom_map.h"
#include"gpio.h"
#include"stdint.h"
#include"prcm.h"
#include"stdio.h"
#include"interrupt.h"
#include"uart.h"
#include"gpio.h"
#include"pin_mux_config.h"
#include"utils.h"
#include"timer.h"
#include"pin.h"
#include"timer_if.h"
//goal vars
extern void (* const g_pfnVectors[])(void);
unsigned int PosEdgeValue[2]={0};
unsigned int TimerOutCont=0;
unsigned char string[];
//defines
#define ccs
//functions
void BoardInit(void);
void UART_Init(unsigned int boand);
void UART_StringPuts(unsigned char *str);
void TIMER_Init(void);
void Sensor_Start(void);
unsigned int Sensor_GetValue(void);
* main.c
*/
#include"hw_types.h"
#include"hw_memmap.h"
#include"hw_ints.h"
#include"rom_map.h"
#include"gpio.h"
#include"stdint.h"
#include"prcm.h"
#include"stdio.h"
#include"interrupt.h"
#include"uart.h"
#include"gpio.h"
#include"pin_mux_config.h"
#include"utils.h"
#include"timer.h"
#include"pin.h"
#include"timer_if.h"
//goal vars
extern void (* const g_pfnVectors[])(void);
unsigned int PosEdgeValue[2]={0};
unsigned int TimerOutCont=0;
unsigned char string[];
//defines
#define ccs
//functions
void BoardInit(void);
void UART_Init(unsigned int boand);
void UART_StringPuts(unsigned char *str);
void TIMER_Init(void);
void Sensor_Start(void);
unsigned int Sensor_GetValue(void);
void TimerBaseIntHandler(void)
{
printf("int_1\r\n");
// unsigned long ulInts;
// ulInts=MAP_TimerIntStatus(TIMERA0_BASE, true);
// MAP_TimerIntClear(TIMERA0_BASE,ulInts);
// MAP_TimerIntClear(TIMERA0_BASE,TIMER_TIMA_TIMEOUT);
Timer_IF_InterruptClear(TIMERA0_BASE);
TimerOutCont++;
printf("int\r\n");
}
int main(void) {
// unsigned int SensorValue=0;
BoardInit();
PinMuxConfig();
UART_Init(115200);
printf("begin\r\n");
//TIMER_Init();
{
printf("int_1\r\n");
// unsigned long ulInts;
// ulInts=MAP_TimerIntStatus(TIMERA0_BASE, true);
// MAP_TimerIntClear(TIMERA0_BASE,ulInts);
// MAP_TimerIntClear(TIMERA0_BASE,TIMER_TIMA_TIMEOUT);
Timer_IF_InterruptClear(TIMERA0_BASE);
TimerOutCont++;
printf("int\r\n");
}
int main(void) {
// unsigned int SensorValue=0;
BoardInit();
PinMuxConfig();
UART_Init(115200);
printf("begin\r\n");
//TIMER_Init();
Timer_IF_Init(PRCM_TIMERA0, TIMERA0_BASE, TIMER_CFG_PERIODIC, TIMER_A, 79);
Timer_IF_IntSetup(TIMERA0_BASE, TIMER_A, TimerBaseIntHandler);
Timer_IF_Start(TIMERA0_BASE, TIMER_A, 0xffff);
Timer_IF_IntSetup(TIMERA0_BASE, TIMER_A, TimerBaseIntHandler);
Timer_IF_Start(TIMERA0_BASE, TIMER_A, 0xffff);
while(1)
{
printf("end\r\n");
// Sensor_Start();
// SensorValue=Sensor_GetValue();
// sprintf((char *)string,"%d\r\n",TimerOutCont);
// UART_StringPuts(string);
// sprintf((char *)string,"PosEdgeValue: 0x%x,0x%x\r\n",PosEdgeValue[0],PosEdgeValue[1]);
// UART_StringPuts(string);
// UtilsDelay(80000000);
}
}
void BoardInit(void)
{
MAP_IntVTableBaseSet((unsigned long)g_pfnVectors[0]);
MAP_IntMasterEnable();
MAP_IntEnable(FAULT_SYSTICK);
PRCMCC3200MCUInit();
}
void UART_Init(unsigned int boand)
{
MAP_UARTFlowControlSet(UARTA0_BASE,UART_FLOWCONTROL_NONE);
MAP_UARTConfigSetExpClk(UARTA0_BASE,MAP_PRCMPeripheralClockGet(UARTA0_BASE),boand, \
UART_CONFIG_WLEN_8|UART_CONFIG_STOP_ONE|UART_CONFIG_PAR_NONE);
}
void UART_StringPuts(unsigned char *str)
{
if(str!=NULL)
{
while(*str!='\0')
{
MAP_UARTCharPut(UARTA0_BASE,*(str++));
while(MAP_UARTBusy(UARTA0_BASE));
}
}
}
int fputc(int ch,FILE *f)
{
MAP_UARTCharPut(UARTA0_BASE,(unsigned char)ch);
while(MAP_UARTBusy(UARTA0_BASE));
return(ch);
}