This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200底层传输Transceiver Mode问题请教

Other Parts Discussed in Thread: CC3200, CC3220SF, CC3220S, CC3220R

目前在做的产品,具有2路以太网和Wi-Fi通信功能,现在需要在以太网接口和Wi-Fi之间建立一个通讯链路,即实现MAC层数据的透明转发功能。原来两路以太网之间已经做完了,现在准备做以太网和Wi-Fi的,想咨询一下,CC3200能工作在AP模式下,允许其他设备连接过来,然后通讯数据通过底层获取转发到以太网接口吗?我看到Transceiver Mode可以访问底层数据,但这个时候CC3200还可以作为AP使用吗?

  • 目前CC3200可以做AP并且只能连接一个Station设备,并且此时只能做AP使用不能同时为Station,以太网的数据可通过发送的数据保存到SPI Flash中,CC3200可以从AP切换到Station模式进行后续的通信处理

    目前TI的CC3200的升级芯片CC3220在AP模式下最大支持4个Station的连接

    WiFi CC3200的升级芯片CC3220的基本信息:

    [数据手册]  http://www.ti.com.cn/product/cn/CC3220?keyMatch=CC3220&tisearch=Search-CN-Everything

    [CC3200S 硬件评估板] http://www.ti.com.cn/tool/cn/cc3220s-launchxl

    [CC3200SF 硬件评估板] http://www.ti.com.cn/tool/cn/cc3220sf-launchxl

    The CC3220 family offers three pin-to-pin compatible variations:

    • CC3220SF: 256kB RAM + 1MB XIP Flash and application level security
    • CC3220S:   256kB RAM and application level security
    • CC3220R:   256kB RAM

    CC3220SF芯片内置了 1MB的Flash,客户的代码直接在Flash中运行,256k的RAM完全开放给客户使用,同时增加了Security的支持

    CC3220S芯片使用256k的RAM同时运行代码和RAM,也就是代码+程序使用的RAM在256k范围之内,增加了Security的支持

    CC3220R芯片内置256k的RAM,

    最新的CC3220升级芯片在AP模式下可以支持最大4个Station的连接,同时增加了IPV6的支持,增强了wifi RF的设计,大幅度提升了SmartConfig的配置成功率,详细了新特性的增加请参考CC3220的芯片手册和设计指南。

  • 芯片信息我了解,我是想咨询一下,在AP模式下能否获取底层的数据包,因为我想实现和以太网接口的透明转发(MAC层数据包)