This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC3200 SPI DMA 的数据传输位问题



想要将SPI DMA传输配置中的数据传输位数从8位改为16位。

通过修改SPI的配置还有修改分配传输通道的位数。

但是我发现这样修改后数据接收不到了。

请问需要如何将8位修改为16位后才可以正常接收数据?

//主机

MAP_SPIConfigSetExpClk(ulBase,PRCMPeripheralClockGet(PRCM_GSPI),
SPI_IF_BIT_RATE,SPI_MODE_MASTER,SPI_SUB_MODE_1,
(SPI_SW_CTRL_CS |
SPI_4PIN_MODE |
SPI_TURBO_OFF |
SPI_CS_ACTIVELOW |
SPI_WL_16));

UDMASetupTransfer(UDMA_CH31_GSPI_TX| UDMA_PRI_SELECT,UDMA_MODE_BASIC,sizeof(g_ucTxBuff),
UDMA_SIZE_16,UDMA_ARB_1,
(void *)g_ucTxBuff,UDMA_SRC_INC_16,(void *)(GSPI_BASE + MCSPI_O_TX0),
UDMA_DST_INC_NONE);