This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教一下 基于SimpleLink WIFI的解决方案 能否在普通路由器上大量连接使用?

Other Parts Discussed in Thread: CC3200, CC3100

我知道普通路由器的连接用户数量是有限制的,根据网上的资料,理论上是253个,和连接用户使用的数据量也有关系,数据量大,无线路由器处理不过来就会掉线什么的。但是SimpleLink WIFI这种物联网应用,数据量是小的,但是接入数量可能比较多。那么我想问:

1) 像SimpleLink WIFI这种应用,一般的无线路由器支持多少个接入?

2) 是否每连一个SimpleLink WIIF设备,就占用一个路由器的用户数?我看到SimpleLink 是有休眠的,在休眠状态下,也占用路由器的用户数吗?还是快速启动后才连接并且占用用户数,而休眠后是不占用的?

  • Q: What are the maximum number of devices that connect to CC3100/CC3200 in AP or P2P mode?

    A: CC3100/CC3200 in AP mode or P2P GO mode supports only one device connected to it at a time
  • 我的意思是CC3100/CC3200 in Station mode的时候,连接到普通路由器上。普通路由器一次能连接多少个CC3100/CC3200 in Station mode?

    另外,CC3100/CC3200 in Station mode连接到普通路由器AP上,从休眠到连接上能传数据,时间要多久?

  • CC3100/CC3200 in Station mode的时候,连接到普通路由器上。普通路由器一次能连接多少个CC3100/CC3200 in Station mode?

    这个取决于普通路由器的能够携带子设备的数量,一般的路由器大约携带32个左右

    CC3100/CC3200 in Station mode连接到普通路由器AP上,从休眠到连接上能传数据,时间要多久?

    如果是NWP网络处理器一致连接AP,那CC3200的M4内核从休眠到发送数据给路由器,大约在ms的时间量级