打搅了
论坛上关于airkiss的资料比较少,我看到CC3200由于只能支持20MHz的频宽,所以对于很多手机路由兼容性不好,请问现在有解决方案吗?CC3220有没有解决这个问题?能否提供一下相关资料说明,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
打搅了
论坛上关于airkiss的资料比较少,我看到CC3200由于只能支持20MHz的频宽,所以对于很多手机路由兼容性不好,请问现在有解决方案吗?CC3220有没有解决这个问题?能否提供一下相关资料说明,谢谢!
20M的问题已经在CC3220里搞定了, 其实老产品即使不支持20Mhz, TI也提供了一种AP模式的配置方法,参考如下link
http://processors.wiki.ti.com/index.php?title=CC3200_Provisioning_AP&keyMatch=provision&tisearch=Search-EN
This user guide describes all the steps needed to use this example, in which the CC3200 device is used in conjunction with a Wi-Fi enabled mobile device running an application (in this case Simplelink Wi-Fi Starter Pro) and allowing it to connect to the Wi-Fi network.
Note: This wiki page is only applicable for CC3200-SDK v1.2.0 and upward releases. For documentation on older SDKs' examples, refer corresponding file in<cc3200-sdk-installation-location>\cc3200-sdk\docs\examples\
The TI SimpleLink Starter Pro application can be downloaded from the App Store (iOS) or Google play (Android).
Note: There are two versions of the SimpleLink Wi-Fi starter applications on the Play Store. Please make sure to choose the “Pro” version.
Provisioning set up is illustrated in the picture below. It consists of the SimpleLink Wi-Fi device being provisioned, a smart phone (Android or iPhone) with TI SimpleLink Starter Pro Application installed and an access point/router (for connection to the Internet).
By default, the page displays all the access points with the name beginning with "mysimplelink-". If the device to be provisioned is named differently, select "Show all", which shows all the access points in the vicinity. And, now select the SimpleLink device to be provisioned. This takes us back to the Configuration page.
If the pop-up page does not show all the Wi-Fi routers, select ‘Show all’, this makes the SimpleLink Wi-Fi device, to send the complete scan list to the phone app.
Select the Wi-Fi router and enter the Wi-Fi network authentication type and password. Press 'Start Configuration' button to start the provisioning process. Several status messages are displayed on the screen, as the provisioning process continues.
In the event of failure, try couple of time by Resetting the device (For 'Reset' button location, please refer to the CC3200 Quick Start Guide)
None