This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200 无法连接

Other Parts Discussed in Thread: CC3200, UNIFLASH, CC3200-LAUNCHXL

用CC3200-LAUNCHXL 的UART做连接口,SOP设置为100,用TI 原厂的CC3200 MOD, uniflash 可烧录文件。但用自己layout的CC3200 模块,uniflash无法连接上模块,下面时format 时的错误信息(COM口设置没问题,同样的设置,原厂模块可烧录)。RX,TX口无外围电路,连接也多次确认无误。

[15:52:51] Begin Format operation.
[15:52:52] INFO: > Executing Operation: Connect
[15:52:54] INFO: setting break signal
[15:52:55] INFO: detecting FTDI for device reset
[15:53:10] ERROR: ---reading ACK signal failed---
[15:53:10] WARNING: ---seting break signal to false failed---
[15:53:12] INFO: setting break signal
[15:53:13] INFO: detecting FTDI for device reset
[15:53:29] ERROR: ---reading ACK signal failed---
[15:53:29] WARNING: ---seting break signal to false failed---
[15:53:31] INFO: setting break signal
[15:53:32] INFO: detecting FTDI for device reset
[15:53:47] ERROR: ---reading ACK signal failed---
[15:53:47] WARNING: ---seting break signal to false failed---
[15:53:49] INFO: setting break signal
[15:53:50] INFO: detecting FTDI for device reset
[15:54:06] ERROR: ---reading ACK signal failed---
[15:54:06] WARNING: ---seting break signal to false failed---
[15:54:06] FATAL: --- Can't connect to device !! ---
[15:54:06] FATAL: Error connecting to the device. Please check your COM port settings. Error code: -3
[15:54:06] INFO: > Executing Operation: Disconnect
[15:54:06] Operation Format returned.

附件是模块线路图。帮忙查看是什么原因,线路?layout?其他?

谢谢!