(1)场景 设备: PC, 路由器,CC3200 开发板。 PC 连接路由器 ,CC3200 作为station模式连接路由器。
现象:CC3200使用DHCP方式分配IP地址正常。请问CC3200是否可以静态分配IP地址,即将CC3200的IP设置为固定的地址(与路由器在同一个网段)?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
(1)场景 设备: PC, 路由器,CC3200 开发板。 PC 连接路由器 ,CC3200 作为station模式连接路由器。
现象:CC3200使用DHCP方式分配IP地址正常。请问CC3200是否可以静态分配IP地址,即将CC3200的IP设置为固定的地址(与路由器在同一个网段)?谢谢。
直接使用API函数
Setting a static IP address to the device working in STA mode or P2P client.
The IP address will be stored in the FileSystem.
In order to disable the static IP and get the address assigned from DHCP one should use SL_STA_P2P_CL_IPV4_DHCP_SET
SlNetCfgIpV4Args_t ipV4;
ipV4.ipV4 = (_u32)SL_IPV4_VAL(10,1,1,201); // _u32 IP address
ipV4.ipV4Mask = (_u32)SL_IPV4_VAL(255,255,255,0); // _u32 Subnet mask for this STA/P2P
ipV4.ipV4Gateway = (_u32)SL_IPV4_VAL(10,1,1,1); // _u32 Default gateway address
ipV4.ipV4DnsServer = (_u32)SL_IPV4_VAL(8,16,32,64); // _u32 DNS server address
sl_NetCfgSet(SL_IPV4_STA_P2P_CL_STATIC_ENABLE,IPCONFIG_MODE_ENABLE_IPV4,sizeof(SlNetCfgIpV4Args_t),(_u8 *)&ipV4);
sl_Stop(0);
sl_Start(NULL,NULL,NULL);