This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200 SDK 1.3.0 在ubuntu下用CCS7.3.0编译时,部分例程编译失败



错误显示

Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed - 5.2.6 [ARM]. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. tcp_socket properties Problems

但是没有找到 ti-cgt-arm_5.2.6 下载途径,能不能提供一下

  • Hi Yaming,

    你可以从如下链接下载相对应的ARM Compiler的版本:

    http://software-dl.ti.com/codegen/non-esd/downloads/download.htm

    也或者按照错误显示的提示进行操作

    ‘Help > Install New Software' and select 'Code Generation Tools Updates'