This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200SmartConfig配置时 红灯亮了 但是我的超级终端怎么显示不出来AP 和BSSID



Host Driver Version: 1.0.1.11
Build Version 0.0.0.0.31.0.0.0.0.0.0.0.0
Device is configured in default state
Device started as STATION
[WLAN EVENT] Unexpected event [0x3]
[WLAN EVENT] STA Connected to the AP: , BSSID: 0:0:0:0:0:0
[NETAPP EVENT] IP Acquired: IP=192.168.1.134 , Gateway=192.168.1.1